My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

Application examples of participants of the manus® competition

En las últimas dos décadas, los Cojinetes de plástico han hecho enormes avances. Hoy, estos avances ofrecen soluciones que reúnen dos nociones opuestas: mejoras técnicas y reducción de costes. El concurso manus® desea recompensar las más audaces aplicaciones con Cojinetes de plástico que resaltan gracias a su eficacidad técnica y económica, su creatividad y sus sorprendentes resultados.
Aquí encontrará algunas de las aplicaciones que nos han sido propuestas.

Search from over 400 applications of our customers


In a wide range of industries, solutions are technically improved and costs saved by the use of plastic plain bearings.


More applications

Plain bearing applications from manus® competition of previous years

iglidur® plain bearing applications from manus® participants

Plain bearing for finger prosthesis

The bearings machined from iglidur J bar stock are corrosion-resistant and have a low wear rate.

Sanding machine for wooden barrels: durable guide rails for grinding head

In this grinding machine for wooden barrels, our lubrication-free linear guides and plain bearings guarantee a long service life.

Gritting unit

The screwconveyer of the gritting unit has to be mounted movable in order to compensate axial offset and dynamic movements in the screw.

Melting probe with iglidur® bar stock

A media-resistant bearing for small installation space was manufactured from iglidur bar stock.

Bearing technology for Mars robots

This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.

iglidur plain bearings reduce friction in a folding trailer

The "Tyligo" folding trailer can be used to transport anything. It contains iglidur plain bearings and 16 iglidur thrust washers.

Maintenance-free shaft guides in doors of high-speed train

At a speed of more than 350 kilometres per hour, these trains will be racing through China as of 2012, connecting Beijing and Shanghai.

Bearing technology and energy chains for electric aircraft

To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.

Plain bearing for seat ski carriage

This innovative sledge allows people to ski sitting down. The sledge is steered by the feet and tilted by the hands.

Electric wheelchair

The TopChair-S wheelchair can climb stairs. The iglidur plain bearings are used in the wheels, which easily cope with the high radial forces.

Plain bearing for all-terrain wheelchair

This manus® contribution also shows an exceptional off-road wheelchair, the "Quadrix".

Linear guide for medical body scanners

A compact and maintenance-free drylin T linear guide system is used in this medical body scanner.

Guide rings for knee joint prosthesis

In this prosthesis for pneumatic knee joints, iglidur® J piston rings replace the previously used PTFE guide bands.

Plain and spherical bearings in the prosthetic joint

This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.

Linear technology for medication dispensers

This machine removes medications from the original packaging and re-packages them in smaller doses.

Linear guides for adjustment unit

A drylin® T-linear guide is used for adjustment. This easily copes with the cycle rate of 80 cycles per minute.

Linear guides for dental casting machine

The closing mechanism of the medical device is supported with a drylin W profile guide at high temperatures and dirt levels.

Guide rings for ice cream filling system

Wear minimised, piston jamming prevented: iglidur® plain bearings replace O-rings in the filling valve of Big Drum Engineering.

Ham cutter

Raw ham is processed in this machine. Since high hygiene standards apply here, self-lubricating iglidur plain bearings are used, which function reliably even after regular cleaning.

Lubrication-free linear and spherical bearings for baked goods gripper

This gripper picks up freshly baked goods from a conveyer belt and packs them in baskets.

Packing robot

Herb drying

This machine is used for preparing and drying kitchen herbs.

Breweries

Plain bearings are used, made of iglidur® A500, an FDA-compliant high-temperature material.

Plain and spherical plain bearings withstand strong vibrations in grain sorters

This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.

Plastic ball bearing for planetary gearbox on wind turbine

xiros ball bearings are used in this plastic planetary gearbox for wind turbines.

Spherical bearing for solar aeroplane

The prototype of the „Sunseeker Duo“ solar plane is the world‘s first solar-powered two-seater.

Plain bearing for parabolic trough system

This solar thermal power plant also obtains energy from the rays of the sun, without fossil fuels.
Further Applications (PDF)

Mesa de calibrado en una máquina sopladora de láminas

Con soluciones tradicionales, durante el proceso de limpieza, el lubricante era lavado o la suciedad era arrastrada en los Cojinetes.

Prótesis de articulación de rodilla

El bienestar del paciente en primer plano - Cómo los Cojinetes de plástico mejoran una articulación de prótesis

Fresadora para tubos de hormigón

La fresadora de hormigón funciona desde hace tres años sin mantenimiento en las condiciones más rudas.

Capota de descapotable

Despliegue automático de la capota: gracias a la utilización de casquillos con valona que pueden ser calibrados, el juego axial máximo pudo reducirse de 1.5 mm a 0.5 mm.

Unidad de bloqueo

Uno de los elementos determinantes para responder a todas las exigencias fue la combinación de Cojinetes de plástico con valona elástica que permitió el montaje exento de juego del gancho enclavador.

Manipulación de sistemas de suspensión

Manipulación de sistemas de suspensión: desde hace un año aproximadamente, el sistema de montaje para sistemas de suspensión funciona todos los días sin ningún problema.

Pivot arm in joining station

iglidur G flange bearings ensure continuous fluid movement in a pivot arm working in a joining station. No lubrication, no maintenance.

Plain bearing for filling valve in beverage bottling plant

El desafío: la temperatura máxima de funcionamiento es de 140°C y los materiales utilizados deben resistir a todos los detergentes utilizados en el sector de las bebidas.

Plain bearing for resuscitation device

This resuscitation device enables optimal cardiopulmonary resuscitation. More than 30 iglidur bearings meet the high requirements for weight and size.

Soporte de montaje

En esta aplicación se utiliza un plato giratorio de polímeros iglidur®, que justamente se destaca por su reducido peso.

Bearing technology for ultra-light gyrocopters

El iglidur® G es la solución ideal para esta cabeza del rotor. Las hélices sustentadoras giran aproximadamente 400 veces por minuto y efectúan movimientos oscilantes de 30° máx.

Plain bearing for wing model

La dificultad de esta aplicación era que los Cojinetes del módulo iban a ser expuestos al agua como medio de medición.

Bearing technology in sports leg prosthesis

Greater flexibility, less bearing clearance and less wear: iglidur plain bearings replace Teflon-coated metal bearings in the Blatchford leg prosthesis

Fully automatic tire fitting lines

No more expensive repairs

Thrust washers for thermal shakers

At up to 3,000 revolutions per minute and 99°C, the iglidur thrust washers prevent imbalances and vibrations and ensure high precision.

Linear guides with no stick-slip effect for a CNC-controlled laser cutting system

This laser cutting system for private households was built to be affordable and low-maintenance. drylin linear guides on the X- and Y-axes.

Plain bearing for solar water pump

Durable and cost-effective: this highly energy-efficient water pump for developing countries is equipped with robust iglidur plain bearings.

Bearing technology for helicopter drone

Light and free from play

Suspension fork Magura

With igus to victory: iglidur plain bearings in the suspension fork from Magura reduce weight and maintenance.

Bearing for quiet vehicle gear

This application serves on the one hand to improve the shifting comfort and on the other hand to reduce the vibration-induced noise in the driver's cab.

Bearing technology for belt conveyors

Efficient with little installation space: linear and pillow block bearings for automatic storage and retrieval units in high-bay warehouses

Adjustable biker's foot rest on motorbike

A drylin W double rail system is installed in this adjustment mechanism for a motorbike footrest, which enables maintenance-free operation even with aggressive media such as salts, dirt and water.

Lowering mechanism for hood ornament

Wear-resistant and secure

Bearing technology for electric motorised gliders

Robust and vibration-reducing


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.