My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

Revolutionary TV mount with PRT slewing ring bearing from igus®: Electric TV mount pushMAXI-TELE+ROTO

Innovative functionality and attractive design for private households and businesses


The pushMAXI-TELE+ROTO from Gruber Systems GmbH is an electric TV mount that uses its versatile functions to perfectly showcase the TV hanging horizontally below the ceiling. The TV can be electrically pivoted from the ceiling to a vertical position with ease. In addition, the electric telescopic function enables adjustment by up to 500mm downwards into the room. The TV can also be manually rotated through 360° using an igus® PRT slewing ring bearings.

The mount is used both in private households and in the commercial sector. In private living areas, it is ideal for larger areas and can be flexibly aligned. When folded up, it provides an unobstructed view through a glass front and hangs unobtrusively from the ceiling so that you can simply walk underneath it.

In the commercial sector, the pushMAXI-TELE+ROTO is often used in meeting rooms, hotel lobbies, fitness rooms and other multifunctional spaces.

Profile

  • What was needed: A slewing ring bearing that allows rotation through 360°.
  • Requirements: It should be pivoting, telescopic and at the same time rotatable up to 360°. In addition, the innovative unique selling points, such as the absence of lubricants to prevent contamination of technical devices, as well as freedom from maintenance and quiet operation for optimum comfort, are desirable.  
  • Industry: Furniture and interiors
Video in German

Problem

During the development of the pushMAXI-TELE+ROTO, one central challenge took centre stage: the space-saving and unobtrusive installation of televisions on the ceiling. Both mechanical functionality and aesthetic design had to be taken into account. 

The main focus was on ensuring smooth running. The TV mount should move silently and smoothly to ensure a pleasant viewing experience. In addition, ease of use was of paramount importance in order to maximise convenience for users. Developing an intuitive mechanism that is both precise and smooth-running was another challenge.

Solution

The PRT-01-50 slewing ring bearing from igus® proved to be the perfect choice, as it enabled extremely backlash-free rotation and was therefore able to cope with the loads and lever forces without any problems. The ease of movement of the bearing in particular played a decisive role.

In addition, the NT-35-AR-520 rail was chosen, which was characterised by its high stiffness when extended. The weight feature and the possibility of full extension were also decisive factors in the decision. It was also particularly advantageous that the rails are now also available in black, which perfectly matches our requirements.

Thanks to the use of the PRT-01-50 slewing ring bearing and the NT-35-AR-520 rail, it was possible to develop a solution that fulfils the highest demands in terms of both functionality and aesthetic appearance.

Products used

Further application pictures

TV mount
TV mount
TV mount

Interactive 3D model for iglidur PRT slewing ring bearing

PRT slewing ring bearings

Tested in the industry's largest test laboratory

igus test laboratory We carry out tests so that you don't have to. Find out how our products are tested in the industry's largest test laboratory. In addition to standard tests, we also carry out individual customer tests. Our facilities for testing applications and materials cover a total of 3,800m².

Frequently asked questions - slewing ring bearing FAQ

FAQ Electrically conductive? Suitable for contact with food? What is the maximum load capacity? You can find answers to these and other questions in our slewing ring bearing FAQ. Here we have compiled the most frequently asked questions about our iglidur PRT slewing ring bearings for you. 


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.