My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

Corrosion-free bearings achieve over 10 years service life in manure spreader

In this boundary spreader, heavy-duty igubal bearings guarantee failure-free operation.

El distribuidor de estiércol AXIS 50.1 W ha sido desarrollado para un rendimiento óptimo.

Nunca más tener que cerrar el grifo y sin embargo poder dosificar con la mayor precisión. Con el AXIS 50.1 W es posible realizar este sueño.
Las cabezas articuladas igubal® de plástico están combinadas con un cilindro hidráulico de la empresa KMF en el dispositivo de esparcimiento localizado. Un test dinámico realizado con 2 veces 100 h por -20°C con una fuerza de bloqueo de 4,000 N refleja una vida útil superior a 10 años. Este resultado destaca las propiedades amortiguadoras de vibraciones y la alta capacidad de carga de las cabezas de horquilla.

En máquinas agrarias, las ventajas de las cabezas articuladas igubal® son:

Libre de corrosión

Económico en comparación con los componentes de acero inoxidable

Profile

  • What was needed: igubal clevis joints
  • Requirements: Corrosion-free as well as heavy-duty bearing components were needed that would function continuously even in cold temperatures.
  • Industry: Agriculture
  • Success for the customer: The igubal bearings were simultaneously put to the test twice over a period of 100 hours each at - 20 °C and under the influence of a block load of 4,000 N. This corresponds to a service life of 10 years. The vibration-dampening specifications as well as the high load capacity and corrosion resistance of the clevis joints contribute to this. They are also a cost-effective alternative to steel bearings.
Discover all products for the agricultural industry
Boundary spreading device in fertiliser spreader

Problem

The fertiliser spreaders from RAUCH Landmaschinenfabrik GmbH, such as the model AXIS 50.1 W in this case, dose with the highest precision when spreading fertiliser evenly on the field. Here, all components used in the fertiliser spreader must be corrosion-free and designed for the high content of ammonia in the fertiliser. This is also the case in the boundary spreading device, which limits the spreading area of the fertiliser to enable more targeted and efficient spreading. Here, clevis joints are used in combination with a KMF hydraulic cylinder, which must be able to permanently withstand the adverse conditions.

Solution

The components used as bearings in the fertiliser spreader today are igubal clevis joints made of plastic. They are combined with a KMF hydraulic cylinder in the boundary spreading device. The high demands placed on the solution in fertiliser technology are demonstrated by the dynamic test that the new system had to undergo. The boundary spreading device was thus put to the test twice simultaneously, each time for a period of 100 hours at - 20°C and under the influence of a block load of 4,000 N. These simulated test conditions correspond to the loads that the system would encounter in practical use within 10 years. The long service life can be explained in part by the vibration-dampening specifications as well as the high load capacity and corrosion resistance of the clevis joints. They are also a cost-effective alternative to steel bearings.

Ver los productos utilizados

Aquí se puede encontrar otras aplicaciones interesantes en otros sectores



Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.