My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

User reports from the railway technology sector

Overview of success stories with products from the areas of infrastructure, passenger and goods transport


Reliable entry systems. When travelling by tram or train, passengers encounter the first igus® components as soon as they board. chainflex® cables, dryspin® lead screw technology and energy supply systems are used to operate entry systems in a maintenance-free and, above all, long-lasting way. Maintenance-free and clean applications in the passenger compartment iglidur® polymer plain bearings and drylin® linear guides ensure clean adjustment, low coefficient of friction and quiet movement without the need for any additional lubrication. This is due to the dry lubricants incorporated in the igus® materials.

motion plastics® are in use everywhere, from the driver's cab to the braking system. The specifications of motion plastics® are also advantageous in the controls that operate trains and trams. drylin® linear guides are used in brake levers, for example. For high wear resistance, bearings in control panels and emergency brakes are equipped with iglidur® G plain bearings. iglidur® plain bearings are also incorporated in the brakes themselves, ensuring perfect function in the event of bumps and dirt. They are also corrosion-free.

Light rail door with igus products

Space-saving light-rail doors with cables and energy chains

Developing compact passenger doors for new light-rail vehicles on the Metro del Valles line in Barcelona is the job of Masats, a Spanish company. Engineers used igus chainflex control cables and e-chains in the door opening mechanisms. The special control cable design allows extremely small bend radii (just 20 millimetres). The cables are thus ideal for passenger doors that are among the most space-saving systems on the market.

Find out more about this application

IdeasTrain: linear bearings for e-scooter lift at Deutsche Bahn

The IdeasTrain is an initiative of Deutsche Bahn dedicated to tomorrow's passenger transport. One of the concepts developed here: an e-scooter lift for space-saving suspension and charging of the scooters during the train journey. The two-wheelers are hooked into a bracket and can be moved up and down electrically on a linear axis. This is where drylin linear systems and drives for lubrication-free operation come into play.

Find out more about this application
Light rail door with igus products

Light rail door with igus products

drylin® lead screw drives keep gap bridging moving on trains

Sliding steps must work in all weather and be safe, so that even passengers with prams or limited mobility can get on and off without assistance. Lubrication-free and thus maintenance-free dryspin high helix lead screws and nuts from igus are central components of an innovation from Knorr-Bremse GmbH, Division IFE. They are resistant to corrosion and media and ensure a long service life ‒ at significantly reduced costs.

Find out more about this application

Maintenance-free shaft guides in doors of high-speed train

These high-speed trains travel between Beijing and Shanghai at speeds of up to 350km/h. The outer doors are guided with shaft guides from the drylin R series. The advantage: the liners of the linear bearings are made of lubrication-free and maintenance-free iglidur. In addition, the bearings move particularly quietly and work reliably even in the sometimes adverse weather conditions.

Find out more about this application
Light rail door with igus products

Incorporated energy chain and smart plastics in train-washing station

Predictive maintenance in a train washing station

The train washing plant belonging to the Société Nationale des Chemins de Fer Luxembourgeois (CFL) cleans local and long-distance trains daily in its 200 metre-long wash hall. To allow the wash trolleys to travel on both sides of a train, several energy chains are used with intelligent sensor technology that monitors the plant condition and plans maintenance predictively.

Find out more about this application

Safe movement of the transfer table

This traverser in the harbour of Felixstowe in England ensures that the locomotives can quickly reach the correct one of the eight tracks. Locomotives weighing up to 170 tonnes are pushed over a distance of up to 30 metres. To guide the cables safely and reliably from the control unit to the traverser, even in the extreme weather conditions and harsh environments, and to keep the maintenance time to the minimum, the operators opted for an igus® flizz® system. This is made of stainless steel in which an E4 series e-chain® and chainflex® cables are used.

Find out more about this application
Traverser with igus energy chain basic flizz

Light rail door with igus products

Lubrication-free linear bearings with high rigidity in a tunnel-cleaning vehicle

For the metro in Riyadh, Saudi Arabia, Zweiweg International developed a two-way cleaning vehicle featuring especially flexible cleaning technology. Linear systems from our modular construction kit also contribute to this technology. The linear technology, which requires no lubrication or maintenance, is compact when retracted, but allows for a long extension that does not yield too much under the high water pressure. Since it is lubrication-free, dirt and dust do not affect its functionality.

Find out more about this application

Railway track testing system

High-speed trains thunder along the tracks at over 300km/h. Even the smallest cracks in the rails can become a safety risk. To locate such defects, Burak Cevik, a Turkish company, is building a testing system that travels along rails. The bearing points use igus® linear plain bearings made of high-performance plastic. The polymer bearings work for many years without lubricants. They are also resistant to dusty and humid environments and fluctuating temperatures.
Light rail door with igus products



Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.