My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

Plain bearings allow clearance-free installation of the locking hook in the vehicle

iglidur plain bearings in locking system for vehicles enable higher process reliability

As part of a project, the task was to design and implement a locking system in the rear area of a vehicle, consisting of six identical locking units. HS GENION GmbH sometimes relies on iglidur bearings here, which enable the clearance-free assembly of the locking hook. Unlike previously used metal-plastic bearings, the iglidur solutions enable the use of fewer parts and a higher process reliability during assembly.

Profile

  • What was needed: iglidur plain bearings
  • Requirements: The list of requirements specifies among other things maintenance-free bearings with a long service life that must be able to withstand high static and dynamic loads and offer both lightness and ease of mounting. A cost-effective solution was also sought
  • Industry: Automotive industry
  • Success for the customer: iglidur bearing enables clearance-free installation of the locking hook; Unlike previously used metal-plastic bearings, the iglidur solutions allow the use of fewer parts and a higher process reliability during assembly
Lock

Problem

HS GENION GmbH offers its technological and development expertise in the field of  automotive engineering as a strategic partner for all development services up to the start of production for the complete vehicle. In the process, ever higher demands are being placed on quality, safety, reliability, service life and costs while reducing the development time of the vehicles. These requirements affect all systems, assemblies and individual parts down to the smallest details.
It also applied to the design and implementation of a locking system in the rear of a vehicle, consisting of six identical locking units. The task was to develop a locking unit that had to meet a number of requirements. It should be maintenance-free, have a long service life, withstand high static stress (at operating temperatures between - 15°C and + 80°C) and high dynamic stress with vibrations, and minimise the risk of wear. In addition, lightness, low noise when working, no clearance, corrosion resistance, easy assembly and disassembly, the number of individual parts (as low as possible) and a limitation of costs also played a major role.

Solution

Our guide rails, among other things, were used in the project planning of the pre-series prototypes. Specifically, the implemented locking unit consists of a guide rail and drive mechanism (part of a pre-assembled module), locking hooks (locking hooks and igus bearing pairing supplied pre-assembled) and a screw shaft.
The advantage of the simple solution is above all the short installation time, which is limited to a simple screw connection. A decisive role in meeting all requirements was the application of an iglidur plastic bearing pairing with a spring-loaded flange, which enables the clearance-free installation of the locking hook. The overlapping of the two bearings was necessary to avoid the possibility of losing them (due to very short insertion length) during transport and handling. In the previous prototypes, metal-plastic bearings and corrugated washers were used. The corrugated washers proved to be a danger to the process reliability of the assembly (small loose parts). An important contribution to reducing the number of parts and simplifying assembly has been made by the screws, which, thanks to their self-locking property, enable the elimination of additional fasteners and securing devices.

"A crucial role in meeting all the requirements was the use of a plastic bearing pairing with a spring-loaded flange, which allows the clearance-free installation of the locking hook. The overlapping of the two igus bearings was necessary to avoid losing them during transport and handling."
 
Alexander Kantor, HS Genion GmbH
Lock


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.