My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

Fish processing with high service life

Hoy en día, el pescado recién pescado es frecuentemente elaborado directamente en los barcos de arrastre. Las eficientes máquinas de recorte y descabezado de la empresa Baader, en Lübeck (Alemania), procesan hasta 32 pescados por minuto (para pescados de 90 cm y 7 kg a lo más).
Los componentes de las máquinas son por lo cual sometidos a una agresiva mezcla de agua de mar y de sangre. En esta aplicación, los Cojinetes de plástico iglidur® exentos de lubricantes de igus® muestran su eficiencia. Los Cojinetes de polímeros libres de mantenimiento son montados en las cadenas de rodillos inoxidables que aseguran el accionamiento entre los grupos principales y secundarios.

Profile

  • What was needed: iglidur plain bearings
  • Requirements: High reliability and freedom from maintenance of all components, as limited maintenance work can be carried out on board the ship
  • Industry: Food industry
  • Success for the customer: Thanks to new stainless roller chains "12 B-2" from Wippermann Engineering with iglidur high-performance bearings in the chain joints, the service life could be significantly increased from 400 to 450 hours to over 3,000 operating hours.
Fishing trawler with de-heading and gutting machines below deck. Fishing trawler with de-heading and gutting machines below deck.

Problem

Fish is processed below deck in two shifts by machines weighing 1.5 tons. The whole thing happens in a sea state, with multidirectional accelerations of up to three times the acceleration due to gravity acting directly on the machines and their components. This also applies to Baader's sophisticated de-heading and gutting machines, which are used on these very ships. The roller chains used to drive the main and auxiliary units of these machines, as well as all other components, are subject to the most stringent requirements. This means that no maintenance work can be carried out on deck. Here, accordingly, absolute freedom from maintenance and reliability of all components applies to the processing of the fish on board the ship. However, the conventional roller chains initially used here were already worn after 400 to 450 hours and had to be replaced. It therefore came as no surprise that the operators quickly started looking for a robust and durable alternative to the previous rol e-chain®.

Solution

Today, the machine builder Baader relies on stainless roller chains "12 B-2" from Wippermann Engineering in Hagen. Thanks to the new solution with Wippermann's "Marathon Chains", an operating time could be increased to more than 3,000 operating hours in the meantime - a significant increase compared to the previous solution. Equally decisive: the chains do not need to be relubricated or retightened. The rol e-chain® owes its enormous increase in service life - without maintenance - to its special link design. A high-performance plain bearing made of iglidur was used in a stainless steel carrier bearing, whereby the tribology of the chain joint was significantly improved. The plain plastic bearing is characterised by extremely high wear resistance, a low coefficient of friction, high compressive strength and resistance to chemicals. In addition, it is maintenance-free and insensitive to dirt. Tests at Wippermann confirmed the selection before it went into series production. In the past, the cooperation has already led to various tailor-made bearing solutions for Wippermann chains. This is because every chain application places different demands on the components involved.

Stainless steel rol e-chain® Stainless steel rol e-chain®
rol e-chain® iglidur bearing in rol e-chain® joint

Comentarios del usuario

Ver los productos utilizados

Aquí se puede encontrar otras aplicaciones interesantes en otros sectores

More information:

Cojinetes deslizantes en cadenas de rodillos

Disminuirá el ruido emitido por su cadena de rodillos con los cojinetes deslizantes de polímero iglidur® tribológicamente optimizados por igus® y libres de lubricantes.


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.