My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

All-terrain vehicle

Lightweight, environmentally friendly and recyclable

What was needed: 
plain and spherical plain bearings

Requirements: 
all-weather, off-road, low-maintenance

Industry: 
automotive engineering

Success for the customer:  
maintenance-free bearings that do not require additional lubricants

Problem:

The designers at Etisoft Smart Solutions were unable to use conventional rolling bearings due to the limited installation space in the transport vehicles. That's why a space-saving alternative was needed. 

Solution:

Polymer plain bearings of the iglidur Z series are used in the control arms of the autonomous transport vehicles. The bearings ensure that the weight of the robot and its load are distributed evenly. They transmit the axial forces exerted on the suspension bolts and ensure that the entire mechanism moves easily.

"For the two most important safety elements of a car, the steering and the brake, we relied on igus plain bearings. The weight advantage and the low maintenance convinces us every time."

Leo Choisel, KG Automobile

Vehicle from KG Automobile

Ample storage space with 520 litres of load volume

The young French car manufacturer KG Automobile relies on the motto "Less Is Better". This vehicle is lightweight, has lower environmental impact and less fuel consumption than conventional cars. The vehicle should also be fun, practical and environmentally friendly.

The off-road vehicle offers a full 520 litres of load volume and a very reliable and maintenance-free modular design. It is also environmentally friendly. Not only because of its lightweight and low consumption. Additionally, the vehicle is produced locally on site at KG Automobile and recycling has played an important role in the vehicle development.

High demands on vehicle and components

KG Automobile's goal was to build a vehicle that is all-wheel drive, has room for two people and weighs less than 300kg. It should be all-weather, off-road, low maintenance and has road permit. A whole range of requirements that made the design phase costly. All components used also had to meet these requirements.

The iglidur plain bearings and igubal spherical bearings from igus were able to enter the race without any problems under these operating conditions. They convince with their mechanical resistance, a very good price and maintenance-free use without additional lubricants. The igubal KSTM pillow block bearings are used for the steering column, igubal KCLM ball heads for the steering track rods and iglidur plain bearings for the brake pedal guide.
Vehicle from KG Automobile

Here you can find the products used




Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.