Metal out, plastic in: igus presents new tribological plain bearings for medium load range08/03/22

iglidur M210 and M260 make bearing points on construction and agricultural machinery free of lubrication and maintenance

igus extends its range of iglidur tribological plain bearings for applications with special loads. The materials iglidur M210 and M260 are new to the range. They enable a quick changeover from thick-walled metal bearings to plastic bearings without any structural modifications. The advantage of a change is that the bearing points no longer require lubrication and are almost maintenance-free. They offer a significant time and cost advantage, especially in harsh environments in the daily operation of construction, agricultural and municipal machines.


The new polymer plain bearings iglidur M210 and M260 offer wall thicknesses of up to 5mm and inner diameters of 20, 25, 30, 40, 50 and 60mm. They are particularly suitable for applications with pivoting movements in the medium load range from 20N/mm2, where a quick replacement of thick-walled metal bushings is required without structural modifications- for example in construction machines, agricultural machines and municipal vehicles that have to withstand harsh environmental conditions on a daily basis. The materials differ slightly but display their different strengths when in interaction with various shafts. For example, the M260 variant achieves excellent wear results in combination with shafts made of St37 steel.

Less maintenance and cleaning effort, more environmental protection
The switch from metal to polymer bearings means significant cost and time savings, especially for machines and vehicles with many bearing points as lubrication is no longer required. The tribological plain bearings M210 and M260 are self-lubricating. Solid lubricants ensure a low friction and dry operation. This significantly reduces the cleaning effort. Because without lubricants, dirt and dust do not have a chance stick. Another advantage: As no lubricants are entering the environment this allows users to contribute to environmental protection. Additionally, the energy consumption of machines and systems is reduced because the plastic bearings are lighter than metal bearings.

Robust and lightweight at the same time
To guarantee sufficient robustness of the iglidur M210 and M260 plain bearings, the material experts at igus work with fibres and fillers. These components strengthen the materials so that they withstand high surface pressures of up to 40MPa and edge loads even under continuous loads - even at extreme temperatures between -100°C and +140°C. Tests in the in-house igus laboratory prove that the polymer bearings show limited visible wear in pivoting movements at medium loads, even after several thousand cycles. "For this purpose, the front loader test stand on the outdoor premises is used. In addition to the standard tests, application tests are vital in material development," says Stefan Loockmann-Rittich, Head of the Business Unit iglidur plain bearings at igus. "All test results then flow into the iglidur online experts, with which the service life of M210 and M260 can be precisely calculated under specific specifications."


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.