Lubrication-free igus linear axis in hygienic design for clean use in food technology17/02/22

drylin ZLW toothed belt axis with FDA-compliant materials can be cleaned quickly and is maintenance-free thanks to tribopolymer technology

The time-consuming cleaning of machines leads to longer and expensive downtimes in many companies in the food industry. To reduce this effort, igus is now launching a ready-to-connect toothed belt axis on the market, which is constructed according to the guidelines of hygienic design. It relies on FDA-compliant materials and the advantages of the lubrication-free and maintenance-free high-performance plastics from the motion plastics specialist.


After mixing waffle batter, clean the bowl and mixing sticks: an unruly business. Large bakeries can tell you a thing or two about it. They face the challenge of regularly cleaning huge vats and mixers - including the linear axes and linear carriages on which the mixers lower themselves into the containers. If classic linear axes are used here, there is a great risk that dough scraps will be deposited in hard-to-reach places, making cleaning considerably more difficult and possibly posing a risk of contamination. "In order to reduce the cleaning of systems in the food industry or even in the pharmaceutical and cosmetics industries, we have now expanded our portfolio of ZLW toothed belt axes," says Michael Hornung, igus Product Manager for drylin linear and drive technology. "The new model can be cleaned particularly quickly and thoroughly - whether with high-pressure steam jets, chemicals or simply running water. This also increases product safety."

Based on the hygienic design cleaning is simplified
The new linear axis is easy to clean because the design engineers at igus followed the guidelines of hygienic design during development. Undercuts in the entire system are minimised where food remnants could accumulate. Likewise, there are no gaps that can occur, for example, if screw heads disappeared into a recess in order to be flush with the surface. "We deliberately avoided countersinking the screws. True to the motto: "Form follows functionality, in this case easy cleaning," emphasises Hornung. Equally important: rounded corners, which ensure that water can flow better during high-pressure cleaning and carry dirt particles along more easily. Water cannot deposit and the formation of germs is reduced. Wherever a dead end was unavoidable, boreholes ensure that liquid drains away completely.

Lubrication-free plain bearings reduce risk of contamination
The igus developers use only FDA-compliant materials for the new toothed belt axis. The shaft end supports and linear carriages are made of corrosion-resistant stainless steel. The plain bearings, on which the carriage moves over the rail, are made of the food-grade tribo-plastic iglidur A160, which enables low-friction dry operation - without external lubricants, which could become a contamination hazard and pollute the environment. This also makes the drylin ZLW toothed belt axis extremely durable. This is illustrated by approximately 1.5 million double strokes at a speed of 0.5m/s and an acceleration of 2m/s² with a load of 3 kilograms, in igus' own test laboratory. The drylin ZLW toothed belt axis can now be ordered with a maximum stroke length of up to 3,000 millimetres and can optionally be equipped with a suitable stepper motor.


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.