Prensa |
|
¿Tiene alguna pregunta? ¿Necesita materiales? Aquí podrá descargar imágenes aptas para impresión y comunicados de prensa actuales. No dude en comunicarse telefónicamente, por correo electrónico o fax. |
|
Contacto para la prensa¿Desea ser añadido a nuestra lista de distribución para medios de comunicación? |
chainflex bus cables save costs with new 300V UL approval15/08/20
The Underwriters Laboratories (short: UL) is an independent organisation in the USA that tests various products for their safety. The regulations with regard to fire protection are very high. Only tested products receive the UL certificate which guarantees easy distribution of the machines and systems worldwide. With regard to cables, the UL stipulates that all cables with different voltage classes in an energy supply system must always be mechanically separated from one another. As a result, the design department has had to spend a lot of time and costs in the designing of the energy chain. To reduce this expenditure and improve technology, igus has now increased the 30V UL voltage to 300V for its CF888, CFBUS.PVC, CF898 and CFBUS.PUR chainflex bus cables and received the UL certificate. This means that cables with the same voltage level can be laid directly next to each other. It is now no longer necessary to separate the cables. "And that can reduce the size of the chain and cut down on the installation work required for separators", explains Rainer Rössel, Business Unit Manager for chainflex cables at igus.
|