Similar price, double the performance: New plain bearing all-rounder from igus29/04/17

igus has improved its best-seller, the all-round bearing material iglide G300, introduced as iglide G1. The new self-lubricating and maintenance-free triboplastic material offers higher temperature resistance and low moisture absorption as well as its improved friction and wear behavior at almost the same price.

When it comes to the minimization of friction and wear without the need for any lubrication or maintenance, customers can now choose from a catalogue that contains a wide range of bearings made of 53 triboplastics with special material properties. In the igus product range, customers can find plastics especially suited for construction and agricultural machines as well as for use in the food or chemicals industry. The most frequently used iglide bearing, however, is iglide G300. Presented for the first time in 1983, it can now be supplied worldwide from stock in 650 metric catalogue dimensions with diameters ranging from 1.5 to 195 millimeters. It combines a favorable price with many attractive technical properties: a long service life across the entire load spectrum on a wide variety of rotating or pivoting shafts, even in very different ambient conditions, for example when applications are exposed to dirt, dust or impacts. At Hannover Messe 2017, igus will now be showing an upgraded version of this successful universalist: iglide G1.

"The new G300": service life doubled

The new all-rounder achieves the stated goals for these igus products, namely enhancement of technical performance and reduction of costs, and does so in an exemplary manner. This is because the material of "the new G300" has considerably improved properties at almost the same price. The igus developers have reduced the wear rates at low loads (up to to 5 MPa) down to levels up to a quarter of what they were before. The service life under heavy loads has almost been doubled, depending on the application parameters. At the same time, the all-rounder can now be used continuously at temperatures up to 180°C (iglide G300: 130°C). In addition, the temperature above which an additional means of axially securing the bearing apart from the press fit is recommended has been increased by half to 120 °C In conjunction with the more than 50 per cent reduction of moisture absorption, this means that the material is suitable for an even wider range of ambient conditions. "The new material is an improved alternative in moving applications where metal solutions have been used up to now", says René Achnitz, Head of Business Unit iglide bearings at igus. "With this new material, customers can reduce costs by around 40 per cent, increase the service life of bearings and, at the same time, profit from the special material properties of iglide such as the absence of a need for lubrication, lower weight and corrosion resistance. "Initially, iglide G1 will be made available in 113 standard dimensions in the form of cylindrical bearings and flange bearings. Moreover, the range of dimensions will now be expanded continually in response to customer enquiries. Thanks to extensive tests in the 2,750 square-meter laboratory, it will soon be possible to calculate and configure iglide G1 online like all the materials contained in the igus catalog.


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.