Mon interlocuteur
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
DE(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

iglidur Q2E: A lubrication-free world for heavy machines19-09-19

In a test, the new high-load bearing withstands up to 130 MPa

In construction machines, agricultural machines, utility vehicles and offshore installations, plain bearings often have to cope with extreme conditions such as heavy loads. igus has therefore further developed its lubrication-free two-component bearing iglidur Q2E The material iglidur Q2 ensures a tested high degree of wear-resistance, and a hard polymer shell protects the heavy-duty bearing.

Dirt, impacts and high edge loads Bearings in construction equipment, agricultural machines and offshore installations often have a hard time and have to cope with extreme conditions. Durable materials and dirt-resistant components are therefore called for. igus has now upgraded its iglidur Q2E heavy-duty bearing for exactly such scenarios of use. igus is expanding its range of bearings for heavy-duty applications and closes the gap between existing bearings and solutions made of metal and composites. The bearing consists of high-performance plastics and is therefore completely lubrication and corrosion-free. The absence of lubrication allows maintenance-free operation of the bearing points and prevents machine failures due to lack of lubrication. Expensive central lubrication systems are no longer necessary. Dirt and impurities can no longer adhere to the bearing points, and this minimises wear. In addition, less grease and oil escapes into the environment, a result of which the annual consumption of over 35 million metric tons of lubricant, as measured by RWTH Aachen University, is reduced. Another advantage: the injection-moulding method used to manufacture the plain bearings is especially cost-efficient.

The combination is the secret
Two materials in an encapsulated design ensure that the bearing can cope even with the most extreme edge loads. This is because the iglidur Q2E has a hard polymer shell and a tribologically optimised core composed of iglidur Q2 as the material. When used for a plain bearing with a diameter of 20 millimetres, this material is also very dimensionally stable and wear-resistant even under high loads of up to 7 metric tons. Functioning as a protective sheath, the shell makes the bearing very sturdy and ensures that it has a longer service life. igus has proven this in its own in-house test laboratory. In the swivel test, the material withstood a radial load of 130 MPa. iglidur Q2E is initially available for shaft diameters of 20, 25, 30 and 40mm.


Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.