Mon interlocuteur
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
DE(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

e-cord micro protects the smallest hoses01-09-14

Modular system from igus to guide and protect very small hoses and cables

Moving small scale capillary tubes reliably and safely often poses major problems for design engineers, especially in the medical industry. igus has now developed the e-cord micro system to address this. The modular system of straight, curved and mounting parts, means that even the smallest tubes can be fitted into moving equipment with confidence.

Medical machines often contain dosing and pipetting functions which require the constant movement of capillary tubes, which are only a millimetre or so in diameter. In these applications the fragile capillary tubes are often squeezed into a small bend radius which can cause damage to the tubes or blockages in the flow through them. igus has designed the e-cord micro to help in these cases. The system ensures the hoses do not fall within a pre-defined minimum bend radius of 45mm, and are also given some physical protection. The modular nature of the system and the elasticity of the material allows machine designers lots of flexibility when designing moving capillary tubes into the smallest of spaces.

Modular Design
igus assembles the e-cord micro to order, ensuring a perfect match to the required motion and space of the machine. In this way, different movement directions and travel path lengths can be implemented easily and flexibly. The concept for the e-cord micro, like many other igus products, was driven by customer requirements for a novel solution to their specific challenges. By producing a flexible solution, many other applications in different industries can be realised too.


Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.