Mon interlocuteur
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
DE(FR)

Minimal wear, maximum hygiene: Plain and linear bearings in filling lines

Self-lubricating bearing technology in beverage filling plants from Küppersbusch GmbH

Küppersbusch GmbH in Velbert develops and manufactures customer-specific filling plants and has been using plain bearings from the igus modular construction system for more than twenty years. A closer look at a manufactured plant shows a wide variety of possible applications for bearing systems made of high-performance polymers in beverage technology.

Profile

  • What was needed: drylin trapezoidal thread, igubal clip bearing, drylin R fixed flange bearing, tribo-tape liner, drylin T rail guide, iglidur flange bearing
  • Requirements: All rotary and linear bearings must be easy to clean and have a long service life. For hygiene reasons, they must not require any external lubricants, and the material of the parts in contact with the product must be FDA-compliant.
  • Industry: Packaging, beverages sector
  • Success for the customer: The bearing portfolio offers components for all requirements: The bearings made of high-performance polymers are lubrication-free, virtually wear-free and FDA-compliant. The users of Küppersbusch systems can therefore do with a minimum of service.
Beverage filling system

Problem

It is frequently small companies in the beverages sector that set important trends and, at least in the beginning, produce smaller amounts. When they want to invest in a partially or fully automated filling system, they often turn to Küppersbusch GmbH in Velbert. A typical feature of Küppersbusch's procedure is that there are no prefabricated solutions or type series. Since most customers want flexible systems in smaller quantities, the solution often consists of semi-automatic, linear filling, labelling and sealing machines.
For all plant components in these systems, it is important that both the rotary and linear bearings can be cleaned easily and achieve a long service life. They must not require external lubricants for hygiene reasons, and the materials of parts that come into contact with the product must be FDA-compliant.
The example of a bottling plant for spirits, which is currently undergoing its final test runs in Velbert before delivery, is a good illustration of how many and which different plain bearings from the igus modular system are used here.
Here, the designers benefit from the constantly growing variety of the iglidur material selection range. Today, instead of the material iglidur A180, the new FDA versions iglidur A181 (blue) and the likewise FDA-compliant high-temperature bearing iglidur A500 are mostly used.

Solution

Height and format adjustments:
For various height adjustments, drylin trapezoidal threads in combination with flange nuts made of high-performance polymers are used (see picture 1 below). The format adjustments are made via drylin R flange bearings (picture 2).
 
Electric motor bracket:
The igubal clip bearings are installed on the bracket of an electric motor to ensure easy installation (picture 3).
 
Vertical linear axis:
On another (vertical) linear axis, Küppersbusch has been using a combination of drylin R fixed flange bearings with aluminium adapters in which anodised aluminium shafts move for many years (picture 4). It does not need any lubrication and is almost wear-free.
 
Rotary table outlet and bottle feed:
The outlet of the rotary table, when feeding the bottles, was originally made of stainless steel. In order to dampen the noise of bottles hitting metal, tribo-tape made of iglidur B160 is used at present (picture 5). The liner is resistant to cleaning agents and is characterised by a very good coefficient of sliding / friction compared to glass.
 
Filling and dosing stations:
At the valves and pumps of the filling and dosing stations, the bottles are drylin T rail guides and connected to the filler. At the centring bridges of the filling tubes, the company installs iglidur flange bearings (picture 6), which are not only FDA-compliant and chemically resistant, but also have an extremely long service life.

"These bearings are heavily stressed. We have a filling machine that has done 40 million cycles and is still operating with the first shaft and the first bushing."
 
Klaus Voigt, project engineer at Küppersbusch on the iglidur flange bearings at the filling and dosing stations
drylin lead screws with flange nuts Picture 1: For height and format adjustments, Küppersbusch often uses drylin lead screws with flange nuts.
Bearing points with plain bearing liner and shaft bearing Picture 2: Three bearing points provide a guidance system here. Liner left and right for shaft bearing, lead screw and nut centred for the drive.
igubal clip bearings Picture 3: Assembly-friendly motor attachment with self-aligning in use: igubal clip bearings.
drylin R fixed flange bearings Picture 4: Visually perfect, low-friction and long-lasting: drylin R fixed flange bearings with aluminium adapter in combination with the matching shafts.
iglidur tribo-tape Picture 5: iglidur tribo-tape (made from iglidur B160 material) at the outlet of the rotary table of a bottling plant.
iglidur flanged bearing Picture 6: FDA-compliant and chemically resistant: iglidur flange bearings on the centring bridges of the filling tubes.

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:



Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.