Mon interlocuteur
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
DE(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

The lightest linear guide in the world at the 2015 Hannover Messe16-04-15

Carbon rails from igus provide "light" run

Hanover/Cologne, April 15, 2015 – Light, lighter, carbon: Whether in the aircraft or automotive industry, when it comes to weight savings, design engineers increasingly rely on carbon fibre reinforced plastic, in short carbon. To meet the demands in this field, igus has developed a drylin W profile made of carbon, which is presented at the Hannover Messe 2015 alongside more than 100 other novelties.


Very lightweight, high stiffness and non-magnetic – these are the main advantages of the carbon fibre reinforced plastic (CFRP) over metal. For applications where these requirements are essential, such as aerospace or medical technology, igus now offers the lightest linear guide in its magnitude made of carbon which is available for up to 2000 mm stroke. Here, it is not only the support material that is made of CFRP, but the whole rail, where the system consisting of rail and carriage is up to 40 percent lighter than one with an aluminium rail and even up to 60 percent lighter than one with a steel rail. This weight saving may constitute money for users, especially in the aerospace and automotive industries. Other industries too where high dynamic movements play a role, such as robotics, are increasingly utilising the weight advantages of CFRP components.

Since igus has been offering shafts made of carbon for more than ten years, the plastics expert has already done a lot of testing and has gathered experience. "Here, it has been shown that iglidur L250 has the optimum wear and friction coefficients in combination with carbon shafts," said Stefan Niermann, head of division drylin linear and drive technology. "According to the test results so far, this also applies to the new rails." Like all products from igus, this novelty is also subjected to extensive tests in order to provide reliable information on the coefficients of friction and service life.

Available as a completely metal-free toothed belt axis
The high profile geometry of the carbon rail enables an attachment by means of clamping jaws, which makes a complicated mechanical reworking superfluous. Moreover, the rail with high profile is the basis for a completely metal-free toothed belt axis, which is available in lengths up to 1000 mm. Here a deflection consisting of a carbon axis, a plastic gear and xiros plastic ball bearings from the igus range is used. Thus, it can be used without restrictions in X-ray equipment in medical technology. Here a major feature is the carbon guide, which like all products from igus does not require any external lubrication and thus is maintenance free.


Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.