Mon interlocuteur
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
DE(FR)

Presse

Vous avez des questions ? Vous avez besoin de documentation ?
Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger.
Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax !
 
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ?

Articles de presse par domaine

igus presents a new energy supply system10-02-15

guidelok slimline P for less weight and more dynamics saves up to 80 percent of the cost

To be able to always achieve faster accelerations and speeds in aisle travels, igus has developed an energy chain supply system completely made of plastic. This is characterised by low weight and moreover, easy installation. Visitors to the igus stand at the Hanover Fair in Hall 17 can experience this innovation and more "motion plastics".


igus has advanced its guidelok slimline system once again and now presents the new GLSL-P, which is entirely made of plastic. The guide system for hanging energy chain applications does not require an enclosed channel trough or other elaborate, expensive enclosures and holds the energy chain system as in aisle travels on the railway. Instead, lightweight plastic segments are mounted only every two metres, which saves up to 80 percent trough costs and also weight compared to the previous metal option. Therefore, even faster speeds and accelerations can be achieved. Another advantage of the plastic novelty is that vibrations are absorbed better. "The lightweight guide rails made of fibreglass can easily be plugged into the plastic segments of GLSP-P, hence, implementing the installation completely without tools, leading to a reduction in costs yet again," explains Christian Strauch, industry manager for materials handling at igus.

Secure hold for energy chain system
Two automatically actuated compensators in the segments of the guidelok slimline P fix the e-chain and ensure a quiet, smooth run. If the chain moves in the radius through the segment, the compensator is activated and fixes the energy chain. The innovative locking levers are complemented by open guide rails made of reinforced plastic between the segments, which allows for more dynamics.


Les termes "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur" et "xiros" sont des marques protégées de la société igus en République fédérale d'Allemagne et le cas échéant à niveau international.

La société igus signale qu'elle ne vend pas de produits des sociétés Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ni de tous les autres fabricants de câbles confectionnés pour moteurs indiqués sur ce site Web. Les produits proposés par igus® France sont des produits de la société igus, réservés aux professionnels.