Presse |
|
Vous avez des questions ? Vous avez besoin de documentation ? Informations presse actuelles et photos à imprimer sont ici à votre disposition, il suffit de les télécharger. Il va de soi que vous pouvez aussi nous appeler, nous envoyer un e-mail ou un fax ! |
|
Contact presseVoulez-vous être ajouté à notre liste de distribution des médias ? |
Fast, safe automation with new e-chain solution for long travels10-11-18
A look at modern production reveals that it is impossible to do without robots. This is most obvious in the automotive industry. Be it as a linear, gantry or industrial robot moving on the 7th axis. In confined spaces and in long travels, they always have to work reliably and quickly. A reliable energy and data supply is required here. With the plane-chain, igus has now developed a novel energy chain system for automation that provides maximum fail-safety in applications with high speeds and cycle rates. In the new concept from the motion plastics specialist, an energy chain is mounted flat on its side in a special trough. The advantage here is that the designer saves space due to the low installation height. The convex bathtub shape of the trough allows the E6 series e-chain to travel securely in two recessed channels. The stainless steel trough with its low friction factor ensures a long service life of the chain. For additional sound insulation of the system, a special plastic insulating layer can be used on the outside of the trough. Thanks to the lightweight components, the e-chain solution can be easily mounted below the ceiling for linear robots. |