My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

The longest travel with plastic energy chain  

The e-chain systems® today clearly contribute toward reliability, as system downtimes, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

LED screen  

Previously used cables from a competitor had failed; since then the temperature-resistant chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

Special machine construction  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

Beverages industry  

As iglidur® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

Fully automatic tire fitting lines  

The previously used bearings were blocked and the shafts used to break. The lubricant-free igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

Concrete pipe cutter  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


Glass processing machine

Delivered complete with guide plate ready to install in a glass processing machine.

Glass processing machine    

Handling system

Robotic handling system for circuit boards. Flexible energy supply system in use in clean room technology.

Handling system    

Glass production

Higher variability at lower costs - Multidimensional energy supply systems raise the performance of robots.

Glass production    

Facade construction

Pivot and rotate with plastic plain bearings - New glass lamellae system / Adjustable facade for the service center of an automobile manufacturer.

Facade construction    

Elevatordoors ”Optilight“

Since most elevator malfunctions are the result of defective doors, an extremely reliable, space-saving solution became necessary here.

Elevatordoors ”Optilight“    

Stop dog system

A stop dog system based on the drylin® W linear guide has been used here for the accurate drilling of glass.

Stop dog system    

Separation of bottles

drylin® SLW - With reverse spindle in the glass industry for separation of bottles.

Separation of bottles    

Washing chain bearings

The reduction of the drive power for bottle washing machines was an important achievement of the iglidur® RN plain bearings.

Washing chain bearings    

Glass cutting machine

drylin® W in adjusting unit for a glass cutting machine.

Glass cutting machine    

Robot for car glass handling

igus® triflex® R has successfully replaced the previous solution attempted with this robot, too.

Robot for car glass handling    

Cutting mechanism

A tarp is lowered slowly over the car, so that at first only the outlines are visible; then the tarp is cut by the special mechanism and the car is presented to the public.

Cutting mechanism    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
We need your post code and country so that we can forward your requests to the right contact person
Postcode:*
Country:*
If you would like to request catalogs or samples then please complete your address here.
Form of address:
Street:
Town:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send