My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

The longest travel with plastic energy chain  

The e-chain systems® today clearly contribute toward reliability, as system downtimes, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

LED screen  

Previously used cables from a competitor had failed; since then the temperature-resistant chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

Special machine construction  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

Beverages industry  

As iglidur® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

Fully automatic tire fitting lines  

The previously used bearings were blocked and the shafts used to break. The lubricant-free igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

Concrete pipe cutter  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


Potato planting machine

Besides the high chemical resistance, the iglidur® J plain bearings offer a maintenance-free dry operation in this application.

Potato planting machine    

Hay spreader

High wear resistance and freedom from maintenance are the main reasons for the application of iglidur® plain bearings.

Hay spreader    

Drilling machine

The completely dry operation and the thereby associated dirt-resistance is very important in the direct application in seeds.

Drilling machine    

Axle bearing

The edge load is frequently a deciding factor for or against the use of bearings particularly in axle bearings for agricultural vehicles.

Axle bearing    

Milking arm

The complete freedom from maintenance in areas of extreme dirt accumulation distinguishes the iglidur® J plain bearing.

Milking arm    

Fertilizer spreader

A dynamic test reflects a service life of over 10 years.

Fertilizer spreader    

Agricultural machinery construction

Compensatory special parts tolerance in rugged agricultural machinery construction.

Agricultural machinery construction    

Gears in vehicles for harvesting sugar cane

Robust under high forces

Gears in vehicles for harvesting sugar cane    

Highly energy efficient water pump for developing countries

Long-lasting and cost-effective

Highly energy efficient water pump for developing countries    

Farm tractor

The suitability of iglidur® G plain bearings in pedal and lever bearing assemblies was proven in a test.

Farm tractor    

Agricultural machinery

In drilling and sowing machines, the plain bearings are exposed to extreme levels of dirt, weathering and shock loads.

Agricultural machinery    

Seed measuring appliance

drylin® N provides free travel path and guarantees the necessary gap.

Seed measuring appliance    

Liquid manure tank truck

Rugged liquid manure tank trucks are used for the economic distribution of biogas manure. In the steered pendular axles, lubricant-free polymer bearings defy all adverse conditions.

Liquid manure tank truck    

Gritting unit

The screwconveyer of the gritting unit has to be mounted movable in order to compensate axial offset and dynamic movements in the screw.

Gritting unit    

Grain sorter

This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.

Grain sorter    

Multifunctional arm for wine-growing

Automated work processes on grape-vines in difficult terrain.

Multifunctional arm for wine-growing    

Production line for fertilisers

Fewer malfunctions under aggressive environmental conditions at this fertilizer plant.

Production line for fertilisers    

Agricultural sprayers

These hydraulic sprayers are used to distribute fertilizers and pesticides.

Agricultural sprayers    

Milking robot

This milking robot can perform its activities around the clock in the open field.

Milking robot    

Harvesting machine

The entire harvest, including fruit packaging in a single process step.

Harvesting machine    

Root ball transplanter

Root ball transplanters are indispensable tools for tree nurseries and for garden and landscaping businesses.

Root ball transplanter    

Single animal livestock scale

xiros® thrust race in a steerable wheel of a mobile hog livestock scale.

Single animal livestock scale    

Cylinders

These cylinders are used in the lifting mechanism of tipper vehicles.

Cylinders    

Muck-spreading cart

This muck-spreading cart is used in agricultural applications.

Muck-spreading cart    

Undercarriage

This under-carriage is used in agricultural machinery as an alternative to air-filled tyres.

Undercarriage    

Disc hoe

This disc hoe makes gardening much easier.

Disc hoe    

Sowing machine

This machine brings seeds for corn, soya or sunflowers to the field to be tilled.

Sowing machine    

Drone

This drone is used for targeted pest control.

Drone    

Heavy-duty applications for igus® bearings in the field

Lubrication-free iglidur® plain bearings ensure a maintenance-free operation and master high loads in agriculture

Heavy-duty applications for igus® bearings in the field    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
We need your post code and country so that we can forward your requests to the right contact person
Postcode:*
Country:*
If you would like to request catalogs or samples then please complete your address here.
Form of address:
Street:
Town:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send