Change Language :

When lighting hoists, video walls, projectors, chandeliers or loudspeakers move vertically on the stage or in the auditorium, the cable package must also be guided safely. If the system is not to be seen or if its weight prevents it from being transported, our e-spool cable drum without a slip ring is ideal. Otherwise, the zig-zag system is a good alternative.

When stage platforms move up and down, all associated cables for drive, media and lighting technology must be move with them. The e-spool allows for energy chain deflections. The zig-zag system is used to supply the follow-up podium with the necessary cables. Maintenance-free iglidur Q3E heavy-duty plain bearings and drylin W linear guides are used for scissor lift podiums.
Like every industry, stage technology has its own specific requirements for machine parts and materials. In this white paper, we give you six tips for the selection and design of vertical energy supply for stage technology


To change the portal section, the portal towers in theatres can often be moved. As the towers are equipped with technology, safe energy supply is necessary. This is where our E4.1 series e-chains come into play. The chain either moves in a trough below the work gallery or hangs freely in a U-shape on the tower.

Scissor hoists are used to open and close curtains evenly, especially with heavy fabrics. iglidur G plain bearings and thrust washers are used in the joints. If the drives for horizontal opening also move, the zig-zag system is a good solution for safely guiding the cables.

If the cable drum is very close to the first guide roller in stage machinery winches, the cable drum or guide rollers must be moved in parallel. This ensures that the steel cables are always guided safely when reeling on and off. Here, our lubrication-free drylin W and drylin R linear guides or a drylin linear axis with lead screw drive are primarily used. In addition, the cable is safely guided in an E2.1 energy chain during movement. The cables are guided on the drum by xiros conveyor rollers, and the drum shaft is supported by igubal® four hole flange bearings with a split housing.

Energy chains ensure safe power supply for moving horizontal elements on stage such as stage trolleys or LED video walls. Our noise-reducing E6 series e-chains or the e-spool cable drum are suitable for this application.

In telescopic spectator stands, cables for the step lighting must be moved by such means as E.21 or E4Q series e-chains. Our maintenance-free plastic slide bearings made from iglidur G or iglidur J are ideal for the bearing points in the seats' tilting mechanism.
Our lubrication-free plain bearings and linear technology components in combination with energy chains for linear and 3D movement ensure that camera dollies, camera sliders and camera cranes move quietly and without vibration and that cables are guided compactly and safely.


Head of Sales Engineering Projects and Installation Service
+49 2203 9649 7439Write e-mailIn person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Friday: 8 am – 5 pm
WhatsApp-Service
Monday to Friday: 8 am – 5 pm