Change Language :
With the experience gained from an application with a travel of over 441m in Malaysia, we started a new project in Antwerp in which twelve STS cranes were equipped with energy chains from the 5050R.17.300.0 series. All energy chain systems installed in a channel in the ground were fitted with stainless steel guide troughs. The travels of these cranes are up to 500 metres.

Download the case study
This case study clearly describes how EMO B.V. was able to achieve running performances of over 375,000km on its STS cranes with igus chains for cranes.