My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

INT(EN)

Safe and reliable in any weather

Profile

  • What was needed: Ready-to-connect energy chain system incl. assembly
  • Requirements: Energy supply as a complete system, weather-resistant, cables with UV resistance
  • Products: e-chain system basic flizz®, chainflex® CF77.UL.DCF34CF9CF10
  • Industry: Science
  • Success for the customer: basic flizz as a complete system, weather-resistant, low-maintenance, cost-effective solution, pre-assembled, long product service life and assembly by igus.

About the application:
A lysimeter system in operation, which has 28 test tanks and a rolling greenhouse. If necessary, the roller greenhouse can be moved over a distance of 21 metres.
basic flizz system

Lysimeter system with 28 test tanks

The challenge

The Ecological-Botanical Garden at the University of Bayreuth has unique installations that are used by scientists for experiments and long-term studies. On 16 hectares of outdoor area and 6,000 square metres of greenhouse space, the garden presents near-natural vegetation types from all over the world and, besides the diversity of plants, shows their ecological relationships and functions. One of the facilities in the Ecological-Botanical Garden is the lysimeter system. With 28 individual experimental basins, it offers scientists the opportunity to quantify the water, nutrient and carbon balance of agricultural crops. In addition, the system is equipped with a rolling greenhouse that automatically covers part of the planted basins when it rains, thus keeping precipitation out. This means that experiments can be conducted with controlled drought stress, which is particularly urgent in view of the increasingly frequent droughts. "In the course of a new research project, we had to modernise the rolling greenhouse at the lysimeter system. It was no longer functional and also didn't meet today's safety requirements anymore," explains Holger Quindt, Electrical Officer at the University of Bayreuth.

Solution

"For the energy supply system in the fully automated rolling greenhouse, we wanted a clean and future-proof solution, so we together decided on a basic flizz complete system," says Oliver Köhler, Sales Engineer at igus. "Apart from that, the use of an e-chain was, from our point of view, without alternative, as a busbar system is not recommended in the outdoor area due to weather and signal transmission. Alternatives such as a trailing cable or a festooning system would have been too maintenance-prone and, in this case, too expensive. Our E2/000 series energy chain was the ideal choice for this application. It is cost-effective, easy to install, very robust and runs quietly over long travels of up to 150 metres." The basic flizz is a complete system and consists of an energy chain filled with the highly flexible chainflex cables from igus and guided safely and without disruptions in a weatherproof enclosure made of stainless steel. The basic flizz system is designed to protect the cable from dirt and extreme weather conditions. The travel of the fully automated rolling greenhouse at the University of Bayreuth amounts to approximately 21 metres. To compensate for misalignments, a floating moving end was installed, which further extends the service life of the entire application. Due to the cross sections and the number of cores, the experts at igus decided to use the chainflex control cables CF9, CF10 and CF77.UL.D as well as the motor cable CF34.UL.D. All cables are UV-resistant and designed for maximum stress. "We have the largest test laboratory in the industry at our command, where we perform over ten billion test cycles per year with energy chains and chainflex cables. This allows us to guarantee reliability, even with long travels, many cycles as well as the most extreme environmental conditions," says Oliver Köhler.
basic flizz system including floating moving end

Fast and easy installation

Another advantage of the basic flizz system is the simple and easy installation. "We dismantled the old energy chain, disposed of the cables and prepared everything for installation. The chainflex cables were delivered to the university pre-assembled with the e-chain. Within one day, we installed the entire system with the help of an igus technician - including trough, e-chain, cables and stainless-steel enclosure. The components of the system are perfectly harmonised, the cables leading to the switch cabinet were precisely the right length and the e-chain with the cables operates safely and centrally in the trough. The easy and versatile installation of the igus e-chains combined with the high stability and long service life of the chainflex cables convince us time and again," says Otto Schmidt happily. Pre-assembly also offers various advantages. Oliver Köhler adds: "When it comes to the automation of machines and systems, there are a number of different reasons to opt for pre-assembled energy supply systems. Production costs are reduced, sources of error are virtually eliminated, project planning takes less time and reliability increases considerably." Holger Quindt from the University of Bayreuth concludes: "We have now obtained a perfect solution. The rolling greenhouse is fully automated, safety is guaranteed thanks to igus and GERLITZ, and we now have a future-proof system that we will be able to enjoy for a long time to come."
New energy chain system
Project team
Customer plant with new system


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH