Change Language :

A data cable is a multi-core cable used for simple transmission of dataand information.It is important that the information moves securely from the sender to the receiver.To ensure that this happens, there are special shielding requirements. igus data cables are used wherever large amounts of data must be safely transmitted in motion. They are usually shielded and carry a wide variety of application signals. Their cores are very thin and have coloured insulation to distinguish them.In the past, these cables were used much more frequently – they are gradually being replaced by bus cables in applications.Of course, they still have their uses, and our customers often deploy them. They are an inexpensive solution for transmitting simple data and are available in various mechanical and electrical designs. The cables are available in three different jacket materials.This selection provides additional savings opportunities.

DIN 47100 contains a colour code for identifying cores in cables. The coding is known throughout all industries, is considered standard and yet not all our cables have coloured cores. Why is that? Coloured cores are standard, but only for very thin cores. At igus we are talking about cores from 0.75mm² and smaller. For thicker cores, black cores with white numbering are used, which are considerably more cost-effective to produce. However, the numbering is difficult to read and sometimes impossible to produce if the core has a very thin cross section. This is why the colour code was introduced to identify the core. For larger quantities of core, additional markings are made on the core using rings, as the quantity of colours is also limited.

Our data cables are not only available in different mechanical qualities, but also in three different electrical designs.We offer our customers three different assemblies because electrotechnical parameters must often be observed when data is transmitted. These special parameters are maintained with the twisted pair construction and the integration of pair shields. The twisted pair construction helps minimize crosstalk between the cores.Stranded core pairs also offer better protection than parallel cores to counteract electrical and magnetic interference fields. The stranding causes disturbances due to magnetic fields inside the cable to largely cancel each other out.If you need a higher level of protection, we recommend cables with paired shields. They provide additional protection against electromagnetic interference between the individual pairs.
What is a star quad structure?
In a four-core cable, this structure describes the arrangement of the cores within the cable. As a rule, coloured cores are in the data cable, but we use the designation 1-4 here to make it easier to explain. In a conventional cable, the cores are labelled in a clockwise direction. This means, for example, that 1 is at the top left, 2 at the top right, 3 at the bottom right and finally 4 at the bottom left. In star quad stranding, the cores are in the order 1, 3, 2, 4 in the cable. The pairs 1-2 and 3-4 are perpendicular to each other in their magnetic fields, which prevents signal overlaps. This avoids near-end crosstalk. You can find more information on this in our blog.
Haven't found the right one yet?
Do you already know our online tool?
Easy to find, select the right type, calculate service life and order online

Product finder
Find exactly the right cable quickly

Service life calculator
Calculate the service life of any chainflex cable

Copper surcharge calculator
Calculate the daily copper surcharge

Configurator for customised cables
Configure your customised cable in just 3 minutes

Are you still looking for an energy chain for your cable?
To the energy chains
... or everything already harnessed?
To the readychain
In person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Thursday: 8 am – 6 pm
Friday: 8 am – 5 pm
WhatsApp-Service
Monday to Thursday: 8 am – 4 pm