Condition monitoring system with smart sensor technology for machine data acquisition
igus® i.Sense: Eliminate unplanned downtime and increase machine availability with smart plastics
"Trust is good, control is better" - smart plastics gives you full control over your systems. smart plastics combine igus high-performance plastics with state-of-the-art sensor technology. The condition monitoring system i.Sense for energy chains and cables consists of several components.
Various sensors are available for machine data acquisition, depending on the application. This means that both mechanical factors such as push/pull forces are recorded as well as electrical ones, such as the cable quality. The connected i.Sense module in the switch cabinet, evaluates all sensor data and triggers follow-up actions. This allows direct input into the machine control system and location-independent visualisation within an online dashboard. It provides the foundations for condition-based maintenance in the smart factory.
The advantages of the intelligent condition monitoring system - i.Sense:
▲ Tech up
Increase machine availability and maximum service life
Better fault analysis thanks to real-time machine data acquisition
Easy to integrate into Industry 4.0/smart factory concepts
i.Sense condition monitoring technology in detail:
Acquire data - Evaluate data - Distribute data
i.Sense sensors
i.Sense smart condition monitoring sensors are used to continuously monitor the operating condition of moving components. They can perform various functions, depending on the application. In energy chains, they are used to monitor push/pull forces (i.Sense EC.P) and to identify chain breaks at an early stage (i.Sense EC.B).
For guided chainflex cables, modern smart plastics sensor technology can be used to monitor the tensile forces on the cables (i.Sense CF.P) and measure cable quality (i.Sense CF.Q) and data transmission rate (i.Sense CF.D). All i.Sense machine data acquisition sensors can also be integrated into the energy supply system at a later date.
i.Sense evaluation module
Subsequently, all supplied sensor data can be evaluated during operation by the i.Sense Module II, which is mounted in the switch cabinet of the system to be monitored. In active fault management, all movement anomalies are detected and directly reported to the user or the machine control system, e.g. Siemens PLC.
With the latest generation, up to four condition monitoring sensors for energy chains and cables can be connected simultaneously with only one switch cabinet module, which means significant savings in space and cost. The new module also offers many typical Industry 4.0 use cases, such as remote resetting via WLAN/SMS and an SMS/e-mail alarm function.
i.Sense connectivity
The i.Sense module offers other network option besides direct integration into the PLC plant control system to prevent total machine failure in an emergency. One is location-independent alerting with the optional SMS module. Another is that all acquired sensor data can be output to an online dashboard.
The condition monitoring dashboard shows at a glance, online or locally, the remaining service life of components equipped with smart technology. The current condition is also displayed in colour using a traffic light code. This immediately gives the system operator a clear picture of the system's condition, enabling him to predictively plan upcoming maintenance intervals.
"Thanks to the digital machine data acquisition and networking of machines and products, we can continuously record component condition and receive a predictive notification as soon as repair or replacement is required."
In international automotive production, the global crane industry, or regional wastewater plants: i.Sense condition monitoring systems are successfully used wherever maintenance costs are saved and machine downtime is prevented:
Condition monitoring systems form the basis for predictive maintenance
smart plastics always gives you the right maintenance strategy
For a solid foundation for predictive maintenance concepts, you need a smart network of individual condition monitoring systems. At igus, everything related to predictive maintenance falls under the term i.Cee. Similarly, i.Sense encompasses all condition monitoring systems.
The central element here is the i.Cee software, which, combined with i.Sense condition monitoring sensors on the energy chain, the plain bearing bushing, or a linear carriage, transform stock products into smart ones. This upgrade creates the capability of determining maximum service life and optimal maintenance intervals in real time based on real usage data.
Condition monitoring with igus: definition, differences, advantages and disadvantages, and many more explanations
What is condition monitoring?Condition monitoring is the regular or continuous recording or monitoring of the condition of a machine (especially for rotating components or moving applications), system, or process.
What is a condition monitoring system?Condition monitoring systems are critical to understanding the behaviour of machines and integral to equipment reliability.
What are the advantages of condition monitoring systems?Most successful examples point to the following benefits: maximised production, increased service life, and reduced maintenance costs.
For this and many other issues, such as condition monitoring systems in the smart factory, overall equipment effectiveness (OEE), and the Internet of Things, and for all the answers to the most frequently asked questions from our customers, see our igus blog: