Solution
The numerous cables, such as fibre optic and signal cables, are now guided in their respective specifications in several
e-spool systems. An e-spool is an energy chain including a drum that can be rolled up and unrolled safely and in a space-saving manner.
The e-spool was used instead of a traditional cable drum because the latter would have required the construction of special cables that would not have been tested in use and whose performance would have been unknown. The e-spool can handle the broad cable mix in full compliance with the project requirements and in conjunction with the multimedia technology.
The e-spool system was installed near the hoisting winches in a machine room. From here, the energy chain is guided to the equipment with a specially designed guide and roller path.
Alfa System also uses our
chainflex product portfolio for moving applications for the cables themselves. The wide range of products enabled the customer to find all the required cable specifications in one place. We also offer a 36-month guarantee on all cables in the portfolio.