My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

INT(EN)

Jacket materials of cables

The outer jacket of a cable provides protection against various adversities such as mechanical stress, temperature or chemical substances with which the cable comes into contact. For chainflex cables, igus offers the jacket materials PVC, PUR and TPE. In doing so, igus ensures that the mixtures of the jacket materials are adapted to the requirements, low in adhesion and highly abrasion-resistant. Depending on the application and external conditions, you can choose between different jacket materials.
 
The PVC jacket is the most cost-effective jacket material, which, by its nature, is designed for low to moderate loads and is ideal for ambient temperatures of +5°C to +70°C. Like all igus jacket materials, PVC is a very abrasion-resistant material mixture for use in the energy chain. PUR, on the other hand, is also notch-resistant and offers high oil-resistance, which is ideal for use in machine tools. In addition, there is an extended temperature range of -25°C to +80°C and a high UV resistance. By contrast, the material TPE achieves the highest UV resistance and oil or organic oil resistance. The temperature range is from -35°C to 100°C.
 
PVC or polyvinyl chloride is a very versatile thermoplastic material and is often used on assembly lines as well as in packaging technology or lighting technology due to its chemical structure and the low flammability of the material. Due to their high strength and good insulation properties, PVC cables are popular even for thin insulation. PVC is resistant to constant moisture and also salt water. In the case of fire in a PVC cable, an additive such as chlorine in the jacket material releases halogens, which can pose a danger to humans.
 
In the low voltage range (up to 1,000V) PVC is also known as the material with the best price/performance ratio. igus offers PVC cables made of non-oil resistant and oil-resistant compounds.
 
PUR or polyurethane, on the other hand, is a halogen-free and self-extinguishing thermoplastic elastomer and has become increasingly important as a cable material in recent years. Up to a certain temperature, PUR is very rubber-like, which makes PUR very interesting for cables, as it is very resistant to bending due to this behaviour. There are the properties of a strong jacket material such as notch strength, low abrasion values and cold flexibility. In addition, its  chemical compatibility is better than that of other materials. PUR cables from igus are resistant to oil and coolant and, due to their composition, do not contain any toxic halogens which could be dangerous in case of fire. PUR cables are a popular material for machine tools, in plant construction, in cement plants, in the paint industry and in the automotive industry.
 
TPE stands for thermoplastic elastomers and is the generic term for numerous subcategories. TPE-U materials are mainly used for flexible cables, since they can withstand mechanical loads very well and are highly resistant to external influences such as chemicals or temperatures. TPE is generally suitable for a temperature range of -35°C to +100°C. In addition TPE is halogen-free. By adding halogen substances, TPE can also be produced as a flame-retardant material and is therefore UL 94-HB compliant. It is often used in energy chains, especially in harsh environmental conditions or applications involving continuous movement. TPE cables are a popular material often used in crane applications, materials handling or low temperature applications.
 
The solutions of the chainflex cables and their areas of application are just as varied and unique as the requirements and applications.

Are you familiar with our online tools?

Simply find and choose a suitable type, calculate its service life, and order it online
Product finder

Product finder

Get to just the right cable quickly
Service life calculator

Service life calculator

Calculate the service life of any chainflex cable
Copper surcharge calculator

Copper surcharge calculator

Calculate the current copper surcharge
chainflex configurators

Configurator for special cables

Configure your individual cable in just three minutes


Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH