Sophisticated bus solution for high data transfer
As automation has expanded over the past few years, data transmission requirements have risen steadily. Distances across which data is moved from sensor to evaluation unit are simple 1:1 connections. Data cables used to handle this. Now they are being replaced, bit by bit, with bus systems, which allow faster, more complex communication within the system. It requires the associated bus cables, which are good at transmitting digital signals with their steep flanks. These cables are, so to speak, special data cables that are built specifically for the requirements of the bus system in question. In the simplest case, this might be colour and core/cross section or certain capacitive or inductive properties that allow the necessary characteristic wave impedance. Today, these cables are the basis for familiar bus systems such as Profibus, Profinet and CAN bus, but also USB and CC-Link. We will show you the features that allow continuously functioning data transmission here.
Buy bus cables