Los Cojinetes igubal® pueden también aplicarse, sin ningún problema, en entornos difíciles. Los casquillos son resistentes a la corrosión en ambientes húmedos o mojados. Las temperaturas de funcionamiento se sitúan entre -30°C y +80°C. Son también particularmente insensibles a la suciedad.
Los Cojinetes pivotantes igubal® no necesitan juntas, incluso en condiciones de contaminación extremas. Esto es válido tanto para el polvo fino como para las partículas gruesas.
This kiteboard has to be able to cope with heavy impact as well as with humidity and soiling.
This aerodynamic steering system is used on hovercrafts.
and the first one that is variably adjustable in its width.
In this packing machine, the boxes are discharged at the end of the process via the ejector unit by means of a pivoting movement.
igubal® pillow block bearing in the stone industry.
Despite high installation costs, the solution with ball bearings and shrink tubing never achieved a proper sealing. The problem could be solved thanks to igubal® flange bearings.
In this case, the use of igus® products is not only advantageous from a technical, but also from a financial point of view when compared to competitive products.
Only extensive earthbound testing can demonstrate the suitability of components for space applications.
Light-weight and mobile robot to inspect pipes on inclines and declines.
As part of a study project, igubal® variable double spherical bearings were used in a robot with parallel kinematics due to the individual pitch sizes in small quantities.
Lubrication- and maintenance-free plastic bearings provide the required functional reliability in electric wheelchairs.
In this air bearing measuring carriage, an igubal® spherical bearing is used because of its fast and smooth precisions.
Maintenance-free igubal® pedestal bearings are used in theatre seats; they are noiseless and operate reliably even at high loads.
For this reason, drylin® linear guides and igubal® KSTM pedestal bearings are used; these need no maintenance and are not affected by the aggressive asbestos either.
igus® bearings are used for the gear shift linkage.
This gate, which can be opened and closed automatically, is used in sport stadiums and is folded like an accordion.
This gripper picks up freshly baked goods from a conveyer belt and packs them in baskets.
When the design was revised, the metal pivoting bearings used so far were replaced by igubal® KGLM pivoting bearings.
Four igubal® pivoting bearings from igus® were tested for the floating axle through the drive, and found to be suitable after several months of tests.
The use of an igubal® EFSM flange bearing has allowed the development of a maintenance-free and silent seat mechanism element.
With this system, for example, terraces can be roofed flexibly. The roof is even waterproof in the closed state.
This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.
This inspection robot was developed especially for use in pipelines.
Since temperatures of several hundred degrees Celsius occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures.
This adjustable camera tripod is usually used for cameras that have their centre of gravity well beyond the bearing axis.
To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.
The special device needed to be as economical as possible in its construction, and the individual components as maintenance-free and durable as possible.
Here, igubal® plastic rod end bearings from igus® are used in the steering on an electric wheelchair.
This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.
This pagepulltester is a high-precision measuring instrument for the bookbinding industry.
This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.
Each machine contains 69 igubal® fl ange bearings, which were chosen on account of their corrosion resistance, lubricant freedom and space-saving design.
With this application, salami is cut into slices. As with all applications in contact with food, here too lubricants cannot be used.
The prototype of the „Sunseeker Duo“ solar plane is the world‘s first solar-powered two-seater.
Previously, metal bearings and linear guides were used, which rusted quickly and therefore required frequent maintenance.
The screwconveyer of the gritting unit has to be mounted movable in order to compensate axial offset and dynamic movements in the screw.
This motor is to drive deep-sea robots even at 6,000 metres under the sea.
igus® thrust washers and flange bearings were used for the new design. They made the elaborate milling of the base plate unnecessary.
the armrests of this chair are adjustable, to accommodate the needs of the individual user.
The steering unit, inclusive of the steering rod, is made of carbon fibres and is mounted with igubal® flange bearings and igubal® rod end bearings. These allow a weight reduction of about 30 per cent compared to other solutions.
Since the tank is filled with salt water, the components used may not be susceptible to corrosion.
En este carrito de golf automotor, los Cojinetes articulados con soporte y los Cojinetes de pedestal igubal® permiten compensar los errores de paralelismo de esta estructura flexible.
En el equipo adicional para el mantenimiento de la césped o para el lavado en exterior, los Cojinetes articulados con soporte igubal® constituyen una solución económica y sencilla para un sistema resistente a la corrosión.
En las máquinas de envolver, las articulaciones igubal® como alternativa a los casquillos metálicos protegen el eje.
Los cojinetes articulados igubal® ponen fin a la corrosión, al mantenimiento y a las alternativas caras de acero inoxidable en los sistemas de accionamiento de las unidades de transporte de la industria alimenticia.
El reglaje de los espejos del telescopio es asegurado prácticamente sin juego por cabezas articuladas igubal®.
Gracias a la ausencia de mantenimiento y de lubricantes, los Cojinetes pivotantes igubal® de la serie de medidas E no permiten interrupciones de funcionamiento debidas a la incrustación de fibras textiles.
Los Cojinetes pivotantes libres de mantenimiento situados en el balanceador de carbón compensan los movimientos del cuadro y de las suspensiones generados por la dinámica de la bicicleta.
Las cabezas articuladas de plástico garantizan un funcionamiento intensivo del equipo.
Tribopolímeros libres de lubricantes en una aplicación extrema - Empaquetadora de perfiles.
Un huevo sobre cuatro ruedas - Cómo las cabezas articuladas y los Cojinetes de deslizamiento de plástico hacen avanzar un vehículo de hidrógeno
Un test dinámico refleja una vida útil superior a 10 años.
Las diferentes combinaciones con cabezas de horquilla de plástico igubal® constituyen una alternativa menos costosa que las cabezas de horquilla de acero inoxidable.
La resistencia a la corrosión y el reducido peso son criterios que jugaron a favor de los componentes igubal®.
Argumentos como la disminución del ruido y la reducción de los intervalos de mantenimiento fueron en esta aplicación decisivos.
La junta esférica igubal® situada entre el motor y la cámara permite aceleraciones de hasta 3 m/s.
Gracias a la utilización de los Cojinetes pivotantes igubal® hechos de tribopolímeros, fue posible reducir el peso del dispositivo de elevación y por consecuente la masa rotacional y la carga del engranaje.
Los movimientos oscilantes y lineares del dispositivo de alimentación son asegurados por guías lineales drylin® y Cojinetes de articulación igubal®.
En esta bicicleta, la conexión entre la rueda trasera y el cuadro es asegurada mediante cabezas articuladas libres de mantenimiento.
Gracias a las cabezas articuladas igubal® libres de mantenimiento, decora sin lubricantes y disfruta cada golosina.
Usados en exteriores, las cabezas articuladas igubal® funcionan absolutamente libres de mantenimiento.
Las cabezas articuladas en los peldaños de caravanas deben ser robustas e insensibles a la suciedad.
La cabeza de articulación igubal® libre de mantenimiento funciona como elemento de unión entre el cilindro neumático y la palanca reguladora.
Las cabezas articuladas igubal® sirven de elemento de conexión en el sistema de dirección.
Sin mantenimiento ni corrosión. Y además, por el color las cabezas articuladas igubal® hacen juego con el cilindro del sensor.
En el soporte de guiado de hilos para el arrollamiento de hilos, los errores de concentricidad y los golpes son compensados por las cabezas articuladas.
Los Cojinetes pivotantes igubal® utilizados son resistentes al medio ambiente y absolutamente libres de mantenimiento.
Por su funcionamiento exento de mantenimiento y su resistencia a la corrosión y a las intemperies, los Cojinetes pivotantes igubal® son empleados en las principales articulaciones de cada persiana.
Insensibles a la suciedad y libres de mantenimiento: las cabezas articuladas y los Cojinetes pivotantes robustos se utilizan en vehículos especiales para el mantenimiento comunal.
Cojinetes pivotantes igubal® como componentes aislantes en los tomacorrientes del metro.
En esta máquina de ensobrado totalmente automatizada a alta frecuencia, las carreras son aseguradas por Cojinetes de pedestal y cabezas articuladas de plástico.
La resistencia al desgaste, a la corrosión y a los detergentes así como una vida útil prolongada eran los criterios decisivos para su empleo en la industria alimenticia.
Los Cojinetes de pedestal de plástico situados en los ejes de accionamiento y en las ruedas dentadas para cadena permiten oscilaciones sencillas y compensan los errores de paralelismo.
La inclinación en las curvas de esta bicicleta "recostada" está asegurada por las cabezas articuladas igubal®.
It is possible to compensate alignment faults with igubal® spherical bearings.
En los equipos de fabricación y de transporte, los Cojinetes de pedestal y los Cojinetes articulados con soporte igubal® compensan los posibles errores de alineación.
La carcasa y la junta esférica universal son ambas hechas de materiales idóneos para el contacto con alimentos.
Las cabezas articuladas situadas en las juntas resisten a los ácidos generados por las uvas.
Esta aplicación se distingue por su larga vida útil y, a la vez, por su diseño apropiado para la industria alimenticia.
Con su pequeño robot, Jonas participó al RoboCup 2006 en Bremen. Con 14 años, ganó el título de campeón del mundo junior en la categoría Rescue Roboter con su construcción.
9.9 million strokes tested without wear.
Tilt-table for turning laboratory specimens.
Las cabezas articuladas y las cabezas de horquilla utilizadas son resistentes a la corrosión y pueden funcionar en líquidos.
Maintenance-free track accuracy
No more expensive repairs
No lubricants in food sector
For wind and rain
Downtimes to zero
Can be handled alone
Light and free from play
Good suspension and economical
Precise and effective
Resistant to wind and rain
Movable and attractive
Light and clean
High positioning accuracy
Maintenance-free and resilient
Los Cojinetes soportan de manera fiable, con reducidas fricciones y sin efecto stick-slip, las altas fuerzas radiales de centraje y minimizan a la vez, gracias a su valona, la fricción al nivel del sistema del brazo.
El desafío: la temperatura máxima de funcionamiento es de 140°C y los materiales utilizados deben resistir a todos los detergentes utilizados en el sector de las bebidas.
El objetivo era mantener el peso de un robot trepador a su más reducido nivel para que el robot sea capaz de desplazarse sobre superficies planas, tales las ventanas, mediante ventosas.
Cabezal de aplicación de un distribuidor de asas.
Un problema que preocupada los constructores era el peso total y las fuerzas de palanca. En este caso era necesario reducir el peso.
Cojinetes de plástico en coches eléctricos para niños: se alcanzó el mayor nivel de calidad.
El iglidur® G es la solución ideal para esta cabeza del rotor. Las hélices sustentadoras giran aproximadamente 400 veces por minuto y efectúan movimientos oscilantes de 30° máx.
Dispositivo de bloqueo en una máquina para el procesamiento de billetes de banco: la articulación doble permite todos los grados de libertad necesarios y soporta a la vez la fuerza de tracción.
Varillaje de dirección del vehículo vencedor de récord HYSUN 3000 con motor de hidrógeno.
En esta construcción era necesario ofrecer un sistema de Cojinetes económico, rígido y una resistencia a la contaminación.
Las cabezas esféricas igubal® son particularmente adecuadas para este tipo de exigencias. Efectivamente, después de 15 millones de ciclos, no dan seña de algún juego notable.
El sistema innovador de carga exterior para helicópteros requería para su construcción un peso reducido, una fiabilidad extrema y, a la vez, una resistencia a las intemperies así como un funcionamiento libre de mantenimiento.
Sistema cinemático para automóviles: los Cojinetes empleados permiten compensar las tolerancias entre el fondo del maletero y el revestimiento lateral.
Sobretodo en aplicaciones bajo el agua, la utilización de Cojinetes de bolas es muy inquietante a causa de los lubricantes. Por razones económicas, las guías de acero fino no son una opción. También por razones de higiene se utiliza materiales plásticos.
Cojinetes de polímeros en máquinas de ensacar hidróxido sódico.
En comparación, los Cojinetes articulados con soporte igubal® eran de lejos la alternativa más económica.
Dado que ni aceite ni grasa deben entrar en contacto con el tratamiento de inmersión, las guías clásicas no pueden ser utilizadas en esta aplicación.
Plain, spherical and linear bearings made of plastic help to improve mobility and the quality of life
Basketball shooting device for wheelchairs: Due to igus® products only a little energy is lost through friction, and there is only a minimal angular shift when the shaft accelerates vertically.
Transfer of the steering movement in a "Body-Turn-Bike" by two rod end bearings.
JAM-08 pillow block bearing and KBRM-08 rod end bearing in a meat portioner / packing device
Truck-mounted customized spraying systems for gardening and tree care companies.
Due to their lower weight and better suspension qualities, the company switched to igubal® rod end bearings.
Polymer rod end bearing in a smoke extraction system at a meat factory.
The spherical bearing used compensates the angle misalignment. That means no more maintenance is necessary.
Used in difficult conditions: vibration, random forces, sudden shocks and cold, wet snow.
Snowboard-like appliance
Mesa lineal de gran calidad equipada con husillos de paso empinado, guías lineales y Cojinetes articulados igubal®.
The aim of the concept is to demonstrate to the students how to handle a programmable logic controller (abbreviation: PLC) in an attractive way.
El robot borrador de la escuela Hans-Böckler incorporada al centro de educación profesional de Münster une técnica e historia cultural.
A pesar de todas las influencias exteriores, los Cojinetes de deslizamiento de plástico libres de mantenimiento aseguran el periodo de funcionamiento necesario.
The unusual design for a recumbent bicycle has got what it takes: cordless screwdrivers are used here to drive it.
Viento, arena y sol: los Cojinetes de deslizamiento de plástico para le técnica solar
New solutions for fitness equipment save production costs and assembly times.
Quick, straight, precise: this is how the requirements in sheet metal machining can be summarized. Sophisticated straightening technology makes all this possible.
Model of a delta robot for the linear optimization of process routes.
Bearings on steering linkage and connection in a racing beer crate.
Linkage on the aileron in a model aircraft - without wear.
Steering/damper connection on a Formula 1 model racing car.
Reliable and vibration dampening linkage on the swashplate and the rotor guide.
Stabilization and alignment of the drive shaft.
Built-in solid lubricants guarantee consistent functionality.
On these horizontal forming, filling and sealing machines, the total freedom from maintenance over the machines' entire life cycle was particularly important for the customer.
Lubrication-free polymer bearing technology for cow cleaners