Expand your modular interface quickly & flexibly with the snap-on-carrier
For even more flexibility in the tightest of spaces
Subsequent extensions or special requests, such as guiding liquid media outside but still close to the interface, are often time-consuming and involve a great deal of effort. This in-house development of the snap-on-carrier can simply be clicked onto an existing igus Module Connect connection in order to attach other components, such as additional cables or pneumatic hoses to the interface in parallel or at a later date.
This means you have all transfer points clearly secured in one central area - and without any tools at all, as the snap-on-carrier was deliberately designed for tool-free assembly. Convince yourself and ask here online for a free sample part straightaway.
Simply attach other plug-in points to the interface
All transfer points at one central location
Cost down
Click and hold
Tool-free installation
Proof
Click onto free fixing slots as required
Secure additional plug-in points with cable tiewraps
Sustainability
Simply add to existing igus® Module Connect solutions
No separate transfer points
Tried and tested in the field:
Module Connect ensures fast maintenance in the packaging industry
In the case of maintenance, igus has provided a plug-and-play system to enable quick maintenance. Previously, maintenance work took about four hours, which could often only be carried out by two employees. A replacement of the energy supply system now takes about 45 minutes with just one person using the new interface concept, the Module Connect from igus.
GHD Hartmann is one of the first customers to use the Module Connect connector. End customers of GHD Hartmann easily replace the energy supply with the plug-in connector from the modular system.
Module Connect adapter avoids long downtimes in automatic parking systems
Wherever fast reaction times are required, e.g in the event of a fault the Module Connect adapter ensures fast connection of the energy supply system to the machine and avoids long downtimes.
For example, in an automatic parking system where the car is weighed and measured by the system and then automatically moved to a suitable parking position.
Where the automation of machines and industrial plant is concerned, there is a whole series of different reasons to decide in favour of pre-assembled energy supply systems.
Manufacturing costs decrease, sources of errors are practically excluded. Less project planning work is needed whereas reliability increases. Possible areas of use are in assembly/installation engineering and handling technology, in conveyor technology or in mechanical engineering.
Move Module Connect into the shopping cart at a click ...
... available from stock!
For users who want to configure their individual interface themselves, there are now Module Connect sets with three or four cable inputs. They consist of carrier housings, connector housings, sealing inserts and strain relief. Accessories, such as single and double locking devices and fixing elements, can be ordered to match the application. Contact inserts for individual configuration are also available at igus!
One connector module instead of many individual connectors ...
... Module Connect
Thanks to the simple modular design, a unique plug-in/disconnect point can be configured as a single module consisting of several different connector housings. Each housing can be fitted with up to four different connector inserts.
The housings can then be joined together, making an almost unlimited number of module variations possible in terms of individual widths and height. Due to the low-profile housing design, the Module Connect saves a lot of space and enables a high contact density for every application.
Request the Module Connect Adapter now Please let us know your requirements and we will develop your individual interface with the appropriate adapter depending on the chain series, width and number of Module Connect connectors.
ONE interface for connecting the energy supply system Module Connect can be adapted to the filling and geometry of your e-chain® and enables ideal cabling in terms of function and design for every application.
Do you need a complete system? From the procurement of all necessary components to the assembly of the ready-to-install system: this way you save up to 95% harnessing time!