High temperature
The temperature resistance of high-performance polymer plain bearings is usually underestimated. igus® plastic bearings prove their suitability at up to 250°C.
After selection of your ZIP code, we designate the relevant staff to attend to you at once.
For more than 35 years, plastic bearings by igus® have been a technically and economically advantageous alternative to metallic plain bearings. Improved by precise additions of reinforcing materials and solid lubricants, they are suitable for applications and requirements of all kinds, reduce maintenance work and allow for technical improvements.
The reasons are obvious – bearings made of high-performance plastics are:
Plastic replaces metal: Save 40% costs – 20 customers will show you how to do it.
100% corrosion-resistant
Long service life and low coefficients of friction regardless of motion type
High media resistance
High temperature resistance
RoHS-compliance
High resistance to dirt
High vibration dampening
Lightweight
Very good price-performance ratio
A classic metal composite bearing essentially consists of a metal cover and a very thin layer of polytetrafluoroethylene (PTFE). Typically, these types of bearing have a maximum wear zone of approx. 0.05 mm or approx. 0.002 inches. During operation, the PTFE layer is worn out. In extreme cases, it is completely worn away until metal runs on metal, resulting in shaft damages or "seizing up" of the bearing.
iglidur® plastic bearings are made of modern polymer compounds, which consist of base polymer, solid particles and so-called solid lubricants. These help reduce the iglidur® plain bearing's coefficient of friction. A transfer to the shaft is not absolutely necessary, but improves functionality. With this homogeneous structure, theoretically the entire wall thickness is available as wear zone.
The oil is absorbed by the body of the porous sintered bearing and provides lubrication, especially at higher rotation speeds. The oil film necessary to ensure that sintered bearings function effectively does not work in the case of slow and/or linear or pivoting movements. In addition, the amount of oil available for the duration of the operation decreases.
The homogeneous and consistent structure with solid lubricating and reinforcing materials but without oil saturation ensures that the solid lubricants incorporated in the material are always available irrespective of the kind of movement. Very low coefficients of friction and wear over the entire life cycle of the product.
Due to the line contact between needle rollers and raceways, needle bearings have – compared to the point contact of the ball bearings – indeed a better load distribution at the contact point during rolling, yet the line contact requires a high Hertzian pressure. Therefore, like all rolling bearings, they are sensitive to vibrations and shocks. In addition, wear of the shafts can occur, which is why usually hardened shafts have to be used. Needle bearings can only absorb radial forces.
Due to the large load-bearing surface and the comparatively elastic properties of the plastic, iglidur® plain bearings are also suitable for heavy shocks and edge loads. Reinforcing fibres provide an additional improvement of the mechanical properties. In combination with iglidur® plain bearings, "soft" shafts can be used in many applications. Even with edge loads, the risk of shaft wear is significantly lower than with needle bearings.
You can quickly find the right product by selecting the application parameters and then calculate the exact service life.
Still unsure? Order our free sample box or an individual sample now and discover solutions for your application.
Would you like an alternative to your existing solution or an individual test setup to convince you of the possibilities with plastic bearings?
More than 140 trillion test movements per year on a floor area of 2,750 m2 – the company igus® tests, analyses and develops its products under real conditions in the largest laboratory in the industry.
The advantages of the lubrication-free plain bearing system in one catalogue – the right material for every application!
Monday to Friday from 7 am - 8 pm.Saturdays from 8 am- 12 pm.
24h