How does the wear in the pivoting develop with increasing loads?
The wear comparison was carried out under the following test parameters:
Load: 1 and 2MPa Speed: 0.01m/s Shaft: Cf53 and 304 SS Plain bearing materials: iglidur J and iglidur W300
Test result
In the igus® laboratories, it was determined that the wear rate of iglidur® plain bearings in the low-load pivoting increases with doubling, but remains significantly below the wear rate of the sintered bushings.
Plain bearings online shop
Choose from more than 8,500 sizes compatible with established plain bearing standards and further established types of bearing.