Driving with hands only: Darios, the digital accelerator ring on the steering wheel
"The accelerator ring is the best-quality product on the market. Its workmanship is superb and its reliability unabated. So far, I have driven a total of 785,000 kilometres without any technical problems. Yes, 785,000 kilometres, or 19.625 times round the world."
This is only one of the many enthusiastic customer references from Darios users. And no wonder, after all, Kempf insists on the highest quality for its products and offers its customers a 30-year guarantee on all its driving aids.
KEMPF was established in 1955 by Hans Kempf, who had difficulty walking after suffering from polio. As an enthusiastic mechanic, he invented the accelerator ring in order to be able to drive with both hands on the steering wheel. By the time he died in 2002, he had retrofitted more than 100,000 vehicles.
The hand accelerator system Kempf developed is the only one on the market that adapts itself to the speed of the vehicle: at low speeds, the acceleration is gentle, progressive, and economical, while at high speeds, it is dynamic so that driving is safer and the driver can perform fast overtaking manoeuvres precisely and easily. All the usual steering wheel functions, such as adjustability, airbag, and horn, are retained. The pedals also remain functional – Darios can be deactivated by means of a switch so that other drivers can operate the vehicle in the usual manner.