Over 6,000 drive cables.
Suitable for 38 manufacturer standards.
Order readycable catalogue 2023

Harnessed cables for energy supply and energy chain

The harnessing of cables according to your individual specifications or industrial standards is one of the core competencies of igus®.
When harnessing cables, the choice of components is also very important for subsequent quality. For this reason, we use flexible cables from chainflex in combination with well-known connector manufacturers such as HARTING, Binder, TE Intercontec, Yamaichi and many others. On request, we can also produce harnessed cables individually according to your wishes and application requirements (no minimum order quantity).
Another advantage of harnessed igus® cables is the large number of jacket materials, which are optimally tailored to the application and will save you money.
 

What we offer you in the field of harnessed cables (readycable®)

Industrially harnessed and 100% tested

100% safety thanks to industrial harnessing

Experience the readycable® factory in its diversity

Harnessed and ready-to-connect cables in energy chains or connected to robots need special properties if they are to function reliably over a long period of time in spite of large numbers of cycles, high speeds, rates of acceleration and challenging ambient conditions. The chainflex cables used for readycable products are intensively tested in the company's own 3,800m² test laboratory, the largest in the industry. The harnessed readycable cables guarantee a long service life thanks to extensive tests and quality inspections in the company's own laboratory and more than 25 years of experience in the manufacture and harnessing of cables.

Why buy harnessed cables from igus®?

Large stocks of electric motors


Large stocks
No minimum order quantity for electric motors


No minimum order quantity
100% tested


100% tested
drylin® E motors have a long product service life


Long product life
Long-term product availability


The product range is available over the long term
Electric motors are ready to ship in 24 hours


Ready to ship within five working days

Further arguments for purchasing harnessed cables from igus

Ready-to-connect directly from the cable manufacturer

Developed for energy chains

Up to 7 price classes with the same electrical properties

All ordered products checked for quality and function

Service life can be calculated online

To your required length: with centimetre accuracy

No minimum order value, from quantity 1

Custom assembly is part of our daily business

3,800m² large test laboratory

Optional with  smart cable monitoring


Why our customers recommend us!

readycable application examples from practice


Sensor for a smart cable | i.Sense CF.P

This sensor has an affinity for cables

For cables that run in an energy chain, a particularly intensive "look" is required: 

  • The CF.P sensor measures the tensile forces on the cables
  • Permanently increased tensile forces can lead to cable damage and in the worst case, cable fire
  • The CF.P sensor identifies maintenance that has been carried out incorrectly on the cables

Move Module Connect into the shopping cart at a click ...

... available from stock!

For users who want to configure their individual interface themselves, there are now Module Connect sets with three or four cable inputs.They consist of carrier housings, connector housings, sealing inserts and strain relief. Accessories, such as single and double locking devices and fixing elements, can be ordered to match the application. Contact inserts for individual configuration are also available at igus!
Go to the shop

Numbers, data, facts about the production of harnessed cables by igus®

Connectors
> than 6,000 connector components in stock
more than 14,000 harnessed cables per week
> than 14,000 harnessed cables per week
14 locations worldwide
14 readycable locations worldwide & > 300 production employees at the Cologne location alone