My contact person
Deepee Industrials Ltd.

11 Ishaga Road Surulere

Lagos, Nigeria

+234 803 3899107
More than 4,600 drive cables.
24 manufacturer standards.

readycable® – the most cost-effective cable that is guaranteed to work

In 7 cable qualities & service life that can be predicted online

Offering around 4,600 harnessed motor, servo, signal and encoder cables suitable for 24 manufacturer standards, igus is the world's No. 1 when it comes to harnessed cables for use in energy chains. Providing seven different cable qualities, the range always offers the most cost-effective drive cable that is guaranteed to work. Thanks to the online service life calculator for ready-to-connect cables, the expected service life for the chosen application can be calculated very quickly. igus is also the only manufacturer to provide a guarantee of 36 months or more than 10 million strokes for its cables.
 

Find & calculate harnessed cables Find the right cable and calculate the service life in 3 steps.
Find & calculate
Industrially harnessed and 100% tested

100% testing thanks to industrial harnessing

The world's No. 1 when it comes to ready-to-connect drive cables for use in energy chains

Harnessed and ready-to-connect cables in energy chains or connected to robots need special properties if they are to function reliably over a long period of time in spite of large numbers of cycles, high speeds, rates of acceleration and challenging ambient conditions. The chainflex cables used for readycable products are intensively tested in the company's own 3,800m² test laboratory, the largest in the industry. The harnessed readycable cables guarantee a long service life thanks to extensive tests and quality inspections in the company's own laboratory and more than 25 years of experience in the manufacture and harnessing of cables.

Ready-to-connect directly from the cable manufacturer

Developed for energy chains

Up to 7 price classes with the same electrical properties

All ordered products checked for quality and function

Service life can be calculated online

Exactly in the desired length (cut with cm accuracy)

No minimum order value or quantity

Ready to ship in 24 - 48 hours

Special forms of harnessing are part of our everyday business

3.800 m² test laboratory


What are the advantages of machine-supported soldering or solder connections?

Find out everything about this topic in the free white paper

If machine engineers and system integrators cannot rely entirely on crimp connections, they have to pay special attention to the quality of the solder connections. That is the only way to ensure constant electric conductivity over a long period of time and to permanently protect the connection point, e.g. against gases or liquids.
 


Why our customers recommend us!

readycable application examples from practice


A perfect match: readycable industry

igus cable harnessing with industrial plug-in connectors by HARTING


Hard rectangular connectors made easy: automated igus readycable cable harnessing of durable chainflex cables with the very robust HARTING industrial plug-in connectors.
 
Whether harnessed control cables within 24hrs from stock or individually tailored solutions from batch size 1 - the thoroughly tested chainflex cable quality combined with the HARTING types of connector Han 3A, 6B, 10B, 16B and 24B as a ready-to-connect readycable solution for industrial applications, helps save costs for time-consuming cable harnessing of the individual plug-in connectors and guarantees reliable and durable components.
 

Find out everything about cable harnessing with HARTING connectors

igus® 2020 news: chain-compatible hybrid cable for the latest motors

Bosch Rexroth MS2N & IndraDrive Mi: now finally the matching readycable® drive cables - harnessed and ready for connection

readycable hybrid

Tech up:

  • Installation space and weight, save weight with the latest hybrid technology: one cable for power and data
  • Can be ordered safely and easily online with a 36-month guarantee
Cost down:
  • Reduced cabling time and effort, only one cable instead of two
  • 24hrs from stock , availability for just-in-time delivery reduces your own warehousing facilities


Sensor for a smart cable|isense CF.P

This sensor has an affinity for cables

For cables that run in an energy chain, a particularly intensive "look" is required: 

  • The CF.P sensor measures the tensile forces on the cables
  • Permanently increased tensile forces can lead to cable damage and in the worst case, cable fire
  • The CF.P sensor identifies maintenance that has been carried out in an incorrect manner due to the cables
  • Data is stored on an SD card and can be read out for analyses


Online Shop

Online shop for readycable harnessed drive cables

Ready to ship in desired length in 24 - 48 hours

Go to online shop

More information on harnessed cables

Free samples

Discover and try out solutions for your applications:

Tested!

More than 1.4 million electric measurements with moving cables are a guarantee of reliability.

News

Minimise downtimes with ready-to-connect cables.

Ready-to-connect energy supply modules

Harnessed energy supply systems: Save up to 80% of process costs.


Consulting

I would be happy to answer your questions personally

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h