Interior separation for all triflex R series
When choosing the right triflex R size, make sure that a clearance space is planned for all electrical, pneumatic and media cables. This is necessary to compensate for forces that occur due to relative movements between the e-chain® and the cables as well as between the cables themselves.
Cables must be installed with sufficient clearance. The following value can be assumed as a rough rule of thumb: the sum of the cable cross sections should not exceed 60% of the effective cross section; in addition, a space requirement of 10% or at least 1mm to the next cable or e-chain® must be observed. The quickest and easiest solution to find the correct triflex R filling is the
interior separation configurator, where all triflex R series are available