My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Search in more than 590 applications

Are you looking for application examples of a specific product tested in practice?
Here you can browse through already implemented applications and filter them according to your specifications.

Product area:
e-chain system®:


High-speed sheet feeding

igus® E6 energy chains are used at Strohmann GmbH. High-speed sheet feeder makes high demands on energy supply.

High-speed sheet feeding    

Clean room technology

No wear in the igus® energy supply system even in endurance tests. In a travel of 290 mm, a number of 50-60 cycles per hour is attained mostly in the three-shift operation.

Clean room technology    

Vibration reducing

The special structure of the chain link and the small division grant an extremely quiet and low-vibration operation of the chain.

Vibration reducing    

Multi-spindle machining center

In this application, a two-spindle horizontal machining center was equipped with particularly silent and low-vibration energy supply systems.

Multi-spindle machining center    

Cutting tool

The igus® e-chain® E6 demonstrates its strengths inthe case of this cutting tool.

Cutting tool    

Temporary display

Visible for approx. only one minute are these pictures, which are ”printed“ with UV lighton a light-sensitive screen.

Temporary display    

”Virtu“ large-format printer

The ”Virtu“ large-format printer can be used to print almost anything: sheetmetal, foils, textiles, wood, glass, and, of course, also paper in widths up3.5 metres.

”Virtu“ large-format printer    

High speed camera positioning

The rail & Tracking systems are used wherever fast camera movements are an important factor as, for example, at sport competitions, but also at many popular events such as concerts, stage shows, etc.

High speed camera positioning    

CNC grinding machine

Incidental grinding residues and the used oil cannot influence the energy supply systems.

CNC grinding machine    

Wafer handling

One igus® e-chain® of the E6 family accelerates the work sequences in the case of this application for wafer handling in the chip production industry.

Wafer handling    

CT scanner

This CT scanner can be used to examine very small animals in vivo.

CT scanner    

High speed camera positioning

The rail & Tracking systems are used wherever fast camera movements are an important factor as, for example, at sport competitions, but also at many popular events such as concerts, stage shows, etc.

High speed camera positioning    

KUKA Cobra

This robot becomes faster, lighter and more compact with an additional axis.

KUKA Cobra    

energy chains for microassembly

Extreme demands on availability and durability

energy chains for microassembly    

Plasma cutting machine

This plasma cutting machine cuts metal plates at maximum speed.

Plasma cutting machine    

Positioning systems for electronics manufacturing

Low vibration, quiet, and low wear

Positioning systems for electronics manufacturing    

Cables in high-speed use

Moving cables in high-speed use - igus energy chain systems in Hekuma plants

Cables in high-speed use    

Low noise: 32 dB(A) ... clean class 1

IPA Class 1 range with new sizes

Low noise: 32 dB(A) ... clean class 1    
Applications overview

I have the following project - following query - following requirement

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
We need your post code and country so that we can forward your requests to the right contact person
Postcode:*
Country:*
If you would like to request catalogs or samples then please complete your address here.
Form of address:
Street:
Town:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send