Smoothie mixing station
Hygienic and fast
thanks to igus® linear axes

With its "Alberts one", the company Alberts has developed an innovative solution to meet the need for healthy food even in stressful everyday life: a robotic vending machine that prepares fresh, healthy snacks such as smoothies, hot soups and vegan shakes on site.

Alberts meets all microbial standards to produce healthy soups and smoothies on site, which consist exclusively of individually quickly frozen (IQF) fruits and vegetables and are free of additives. Only pure water is added within the device, resulting in a snack full of nutrients and a sugar content of <5%. 

Alberts' free mobile app allows consumers to share their recipes and experiences with the healthy snacking community. A health coach integrated in the mobile app gives consumers personalised advice based on their own nutritional needs and daily habits. 

Profile

  • What was needed: Lead screw axes, toothed belt axes and linear rails
  • Requirements: A cost-effective and scalable solution for the vending machine that can simultaneously ensure food safety and handle low temperatures.
  • Industry: Vending machinery
  • Success for the customer: Our axes, in combination with motor and control system, ensure a cost-effective turnkey solution that meets the requirements.
More application examples
healthy vending machine

Products used

Configure lead screw axis

Are you still looking for the right linear module? Configure your desired product now.

Problem

In the search for suitable components for the Alberts One, real all-rounders were sought. The company was looking for guidance that was compact, quiet, low-maintenance, temperature-resistant, hygienic and quick to clean.

The biggest challenges for Alberts were to maintain the quality of the food and at the same time develop a robotic vending machine that was technically perfected and yet cost-effective. Especially in view of the costs, implementing a full-fledged robot arm was out of the question. This would result in immense costs, which would mean that the full potential of the machine would not be exploited. We were looking for a lean and scalable solution.

But there were also other technical challenges that needed to be solved. Electromechanical solutions were sought that could work efficiently even at -18°C. Furthermore, the components had to be particularly space-saving.

Solution

The number of degrees of freedom was reduced to a minimum and the highly complex system was optimised to ultimately arrive at a marketable solution concept. Through in-house development, Alberts managed to develop a machine that can work in the deep-frozen sector, while also reducing costs by €15,000, which now makes the machine cost-effective by more than half the price of some of the competitors' machines.

The horizontal movement of the robot arm takes place via the drylin® W linear rail. It is made of anodised, corrosion-free aluminium and is characterised by a flat design. The robot arm moves on it, which in turn is mounted on a drylin® W linear carriage, driven by a toothed belt. The chainflex® control cable, designed for a particularly narrow bend radius with limited space requirements, follows the movement in an energy chain made of high-performance plastic. 

All igus® components are free of lubrication and thus reduce maintenance costs. A system was developed with the help of the igus® parts, which also has low vibration and is ideal for use in the food industry.

Impressions


More application examples


Drive technology online shop

Drive technology shop Order finished linear modules in standard sizes directly online.
Go to the online shop

Drive technology configurator

Drive technology configurator Haven't found the right product yet? Configure your own linear unit.
Go to the configurator

Download whitepaper

Drive technology white paper Lead screw drive or toothed belt? How to find the right linear module
Download whitepaper