My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

INT(EN)

Lightweight and maintenance-free pillow block bearings in the rotor head for ultralight gyrocopters

Reliable and vibration-dampening: iglidur plain bearings and igubal pillow block bearings in the rotor head

iglidur G is the problem solver for this rotor head. The rotor blades rotate approx. 400 times per minute and perform oscillating movements with a maximum of 30°. The support consists of two plastic plain bearings and two thrust washers made of iglidur G. Further bearings absorb the rotary movement of the brake lever. And two igubal pillow block bearings are provided for the control system, which dampen vibrations and compensate for misalignments.

Profile

  • What was needed: iglidur plain bearings, igubal pillow block bearings
  • Requirements: A lightweight and reliable bearing for the rotor head and brake lever was sought.
  • Industry: Aerospace, aviation industry
  • Success for the customer: The decision for the bearings resulted from several reasons: They are particularly vibration-dampening, insensitive to dust, low-maintenance, compact and especially light. In addition, they have high strength values and convinced the customer with their low cost.
Rotor head

Problem

For this ultra-light gyroplane, Schwarz Industrieservice was looking for a suitable bearing for the rotor head. The rotor blades rotate dynamically at approx. 400 revolutions per minute, performing oscillating movements of max. 30°. A grease lubrication device is provided for this purpose. The gimballed rotor head can be steered around the longitudinal and transverse axis. Only occasional steering movements occur in the process. An initial filling with grease is sufficient. A rotor brake must brake the rotor speed from approx. 200 revolutions per minute to standstill. The rotary movement of the brake lever also had to be supported.

Solution

For the bearing of the longitudinal and transverse axis of the rotor head, four plain bearings and thrust washers made of the material iglidur G were chosen. Two iglidur plain bearings were also used for the rotary movement of the brake lever for the rotor brake. The braking torque is absorbed by two iglidur thrust washers. For the control of the rotor head, two igubal pillow block bearings are used, which are vibration-dampening and compensate for misalignments.
The decision for the bearings resulted from several reasons. It is particularly vibration-dampening, insensitive to dust, low-maintenance, compact and especially light. In addition, they have high strength values. Finally, the cost-effective prices were also convincing for the choice of the iglidur G plain bearings.

Rotor head


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus GmbH or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH