Change Language :

As a manufacturer of high-performance plastics, the sustainable and resource-saving use of plastic is very important to us. Therefore, with chainge, we have created a programme for the circular economy to make the recycling of engineering and industrial plastics particularly easy. Recycle your old energy chains from igus and other manufacturers free of charge with chainge. You save transport and disposal costs, receive a certificate for the recycled quantity and the CO2emissions saved, and can be sure that the material will be returned to the circular economy. Become a chainger now!
In production, it is relatively easy to recycle waste, such as sprues and rejected parts. This so-called post-industrial waste is generally unmixed and uncontaminated, which means it can be processed easily and without complications. However, the situation is different for post-consumer waste, i.e. products that are disposed of after use. Here, there are often no options for sustainable reuse.

In 2019, igus wanted to offer customers the option of returning plastic energy chains for recycling when they had reached the end of their service life. Our chainge programme was created from this desire. The interest and commitment of our customers for this programme was overwhelming and motivated us to think big about recycling. With chainge, you can now recycle not only igus energy chains, but also those from other manufacturers. You can register the used recyclables quickly and easily for recycling; collection and recycling are free of charge for you. You will receive an annual certificate detailing the amount of recycled material and the CO2 emissions saved. Since the start of chainge, we have already recycled over 251,000kg of material.

igus energy chain E2

Schwarze Energiekette von anderem Hersteller

Energiekette ohne Fremdteile
At chainge, all energy chains made of PA6 (polyamide 6) can be recycled. Foreign parts such as mounting brackets, rol e-chain links or cables must be sorted out beforehand and the chains must be clean or only lightly soiled.

igus e-skin and e-skin flat energy chains

Energieketten von anderem Hersteller mit farbigen Elementen

Stark verschmutzte Energieketten mit Fremdteilen
Energy chains that are made of a different material than PA6 (polyamide 6) , contain foreign parts or are very dirty cannot be recycled by chainge. These include, among others, the following chains:
Sustainable action is an important topic that we want to promote in the German economy. To this end, we have created a white paper that explains the most important terms for correct recycling and shows the importance of plastics, including recycled plastics, in Germany. In addition, our chainge programme also presents a simple way to recycle technical and industrial plastics to support the circular economy.

The recycling material from our chainge programme, along with other recycled plastic products, flows into our material igumid CG LW, a further development of our recycled material igumid CG. Following extensive testing at our test laboratory, we completely switched the E2.1 energy chain series to this new material in 2025. This reduces the CO2 footprint by 80% compared to the standard material.


Since the launch of chainge in 2019, we have already recycled over 251,000kg of material and returned it to the circular economy. Many different customers have participated in our programme and put their trust in us. They have become chaingers, as some particularly positive feedback below shows:
In person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Friday: 8 am – 4 pm
WhatsApp-Service
Monday to Friday: 8 am – 4 pm