Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

igus humanoid ready for the World Cup02/01/2016

The motion plastics specialist supports designers in new fields of research and application of low-cost robotics

A joint project of the University of Bonn and the Cologne-based company igus GmbH shows that the applications of robots are not just limited to industrial purposes. A humanoid robot was designed and steadily developed over the last two years. The project demonstrates future possibilities in the field of robotics beyond classical industrial applications.

For over two years, a research group of the University of Bonn and the motion plastics specialist igus have been collaborating in the development of a humanoid robot. The robot has already won the RoboCup soccer championship in 2012 as well as the RoboCup Design Award in July last year. Now it has gone another step forward in its evolution and now has new potential in terms of autonomy and fluid motion. It can now can visually detect a football, approach it and strike the ball into the goal. The body elements, made of plastic designed by igus, support and protect the robot when tackled. If this results in a fall, the latest version of the robot is capable of standing up by itself again from the prone and supine positions as well as from on its side. In this way, the igus humanoid already has the best prerequisites for a successful participation in the RoboCup Soccer World Cup next year.

Presence of future robots in everyday life
The design and engineering of the outer shape as well as the supporting parts were contributions from igus, and were produced using the laser-sintering process. In the next advancement energy and data shall be safely guided inside the robot with the help of chainflex cables. The project illustrates new applications for robots. In this way the use of a similar humanoid is conceivable in the area of domestic help in the future. igus has been active for years in the field of robotics and low-cost automation. For example, the robolink D enables the implementation of individual and cost-effective robotic concepts by means of a directly driven articulated arm made of plastic and aluminium. Customers can profit from low costs and the advantages of motion plastics from igus: Low friction and wear coefficients, low weight and freedom from lubrication and maintenance.

The igus humanoid in action: https://youtu.be/QeP_Df5CNQQ

igus® products are available from 24h. The delivery time for energy chains is 24-48h. However, due to peak order levels, the delivery time for energy chains is temporarily 5 to 10 work days. We are working intensively to quickly remedy this situation.