Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

Energy chain solutions for fast rotational movements, from stock06/01/2016

Some solutions that were originally developed as a solution for a specific customer requirement, often find their way into the igus standard range. In this way the motion plastics specialist often developed solutions that would be interesting for another customers too. "We often develop new products by working closely with customers in search of new solutions and by actively asking for the problems faced by users," explains Frank Schlögel, Head of Engineering Projects at igus. "This is the case with our RBR systems for circular motions."

Two-piece trough for quick rotations and low displacement forces
In the rotary modules, the energy chains are mounted on the side and use a "reverse bending radius" (RBR). This means that the chain links can be moved in both directions, unlike conventional linear travels. The cables and hoses are securely guided in the chain with locking separators. With 1,040 abrasion-resistant chainflex cables, igus also offers a complete range from stock to guarantee maximum service life for moving applications. For rotary modules with high speeds and many motion cycles a two-tiered guide channel is used. One part is fixed to the static point of the system, the other to the rotating point. In this way the fixed end of the energy chain can be freely selected. "We minimise the relative movements of the cables and the energy chain through the split guide trough," explains Frank Schlögel. "As a result, we achieve better reliability and minimise the forces in the chain." For applications with lower speeds igus provides rotary modules with static guide troughs.

Flexible use of the design space The standardised modules from the catalogue can be delivered within two weeks. In this way the lead time required for a special project is also eliminated. Depending on requirements, they can be supplied with optional mounting brackets or a cover. In systems with high lateral accelerations or systems that operate in a "tilted" position, the carried guide elements provide additional security and protection to the energy, data and media guidance. For environments with extreme dirt accumulation, for example in open cast mining, cement works or in coal terminals, the use of an enclosed trough is also possible. In this way, dirt which falls within the working range of the energy chain exits again and does not accumulate in the guide trough. And for applications with very small installation spaces, opposed energy chains can be used to save space.

Depending on the selected diameter, rotation angles from 420 to 600 degrees and rotation speeds up to 360 degrees per second are possible for the modules. Thanks to the flexibility and speed of the system, and the flexibility in the design, the modules are suitable for a variety of applications. From traditional mechanical and plant engineering through to high-tech applications in satellite antenna construction or in giant offshore applications, rotation angles up to 900 degrees can be implemented by combining multiple RBR systems. And if customer applications exceed the requirements of the standard range, igus is continuing to focus on customer-specific solutions in order to offer the best solutions for users.

Because of current order peaks our lead-time will increase temporarily to 6-12 working days for e-chain systems®. We are working intensively on a fast improvement.

igus® contact +49 (0) 2203-9649-0 Send e-mail to igus®

myigus myCatalog

Press releasesPress contactInclude into the press distribution list

No minimum order value
700 - 2000 Delivery+Consultation Delivery from 24h* Free samples

More than 100,000 products available! Delivery and consultation Mon-Fri from 7am-8pm and Sat from 8am-12pm!

Newsletter Registration
Terms and Conditions Imprint General Information Data Privacy Protection Declaration