Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

No lubricant, no bacteria: New material from igus for medical technology16/11/2015

Lubrication-free, media-resistant, non-magnetic, corrosion-free - these are decisive criteria for components in medical technology. From pick & place equipment in the laboratory to mechanical joints on patient furniture, the application areas are very diverse in this industry for products in motion. However, antibacterial components are also becoming increasingly important for devices and machines. The motion plastics specialist igus has developed the new material iglidur AB specifically for antibacterial plain bearings, which will be presented to a professional audience at Compamed. According to the test results for antimicrobial efficacy according to ISO 22196: 2011 (the measurement of antibacterial activity on plastics and other non-porous surfaces) the bearings made of the new material help to reduce the bacterial contamination for users or patients. Like all products from igus, the iglidur AB plain bearings also operate completely without external lubricant. "That brings two advantages to the medical and laboratory technology," explains Ulf Hottung, industry manager for medical technology at igus. "On the one hand there is no risk of contamination by oil or grease. On the other hand machinery and equipment can be cleaned safely, without the risk of washing away lubricants."



Antibacterial plain bearings available from stock It is also important for the cleaning of machinery or equipment, especially in the medical technology, that the components are resistant to media. The new iglidur AB plain bearings have a good resistance to chemicals, which is why the contact with aggressive cleaning agents is also not a problem. The plain bearings made of the new material are already available from stock at igus in six different dimensions. A continuous application temperature range of -40 to +70 degrees Celsius is possible with plain bearings made of iglidur AB.

Because of a current peak in orders, our delivery times have increased temporarily to 6-12 working days for e-chain systems and chainflex® cables. We are doing all we can to reduce delivery times as quickly as possible.

igus® contact +49 (0) 2203-9649-0 Send e-mail to igus®

myigus myCatalog

Press releasesPress contactInclude into the press distribution list