Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

Selective laser sintering with igus: SLS powder for wear resistant components in motion26/11/2015

The process of 3D printing is booming and for a while now it is not only hobbyists who have been printing special geometries for self-made projects. Corresponding components are used today as standard in the industry. In order to offer more and more product variety to the users of this technology, the motion plastics specialist igus has now presented the first SLS material iglidur I3-PL. In addition to the four already available tribo-filaments for the FDM process, the new tribo-powder is remarkable with good wear coefficients. "The laser sintering is known in 3D printing for a much higher precision compared to the FDM process," explains Tom Krause, product manager at igus. "Another advantage of our new material is also that the parts can achieve a much higher strength due to the pressure in the SLS method." In laser sintering, no support structures are needed, as the loose powder that is not melted by the laser, acts as a support material. Thus less finishing work is needed on the components and the finished parts can be used directly. In the test laboratory at igus, plain bearings made from the new material have been compared with common materials for selective laser sintering. Both in pivoting, rotating and linear motion, the parts were at least three times more abrasion resistant than the compared materials. In the current beta phase, wear-stressed components are tested in customer applications in addition, other interesting applications have been sought for the SLS print by tribo-optimised components.

Printed parts supplied on request Those who have no 3D printer available can use this technology anyway, for example, for prototypes or special parts in small series: because for such cases igus provides a 3D printing service for the materials iglidur I180-PF, iglidur I180-PF BL, iglidur I170-PF and iglidur J260-PF. A printing service is also being planned for the new SLS material iglidur I3-PL. Customers can get their components printed and delivered quickly. For the print service all we need are the CAD models The price and the delivery time will vary here depending on the complexity of the components. The delivery time target is, however, 'from 24 hours'.

igus® contact +49 (0) 2203-9649-0 Send e-mail to igus®

myigus myCatalog

Press releasesPress contactInclude into the press distribution list

No minimum order value
700 - 2000 Delivery+Consultation Delivery from 24h* Free samples

More than 100,000 products available! Delivery and consultation Mon-Fri from 7am-8pm and Sat from 8am-12pm!

Newsletter Registration
Terms and Conditions Imprint General Information Data Privacy Protection Declaration