Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

iglidur Q290: robust and delicate on soft shafts03/11/2015

In the building and agricultural industries, difficult conditions are the order of the day: environmental aspects, mud and high levels of stress have an adverse effect on machines and vehicles. The new iglidur Q290 material is a specialist among the iglidur materials and is specifically designed for this area of use. Low friction and resistance to dirt are among its strengths. As there is no need for lubrication, igus bearings are always ready for action, even is machinery has been at a standstill for long periods of time Thanks to the new material, the absence of lubricant means that there is no chance of contamination within the soil when work is being done in the field.

Cost benefits for agricultural equipment For the agricultural industry, the price/performance ratio is also a strong argument in favour of iglidur Q290. For example, compared to iglidur Z, a material that is also designed for high levels of stress, the new material is less expensive and is specially tailored to the requirements of the industry: "Fitted in agricultural equipment, bearings are often subjected to slewing movements on galvanised shafts. Compared to iglidur Z, which works well in extremely difficult conditions, for example in respect of the temperatures of an application, what is so convincing about the new iglidur Q290 material is the more than fifty per cent less wear on galvanised shafts", explains Uwe Sund, Industry Manager Agricultural Technology at igus. iglidur Q290 thus demonstrates that specialised solutions enable the customer to achieve cost savings. The material is now available from stock in six different inner diameters up to 50 millimetres, quantities of 1 and more can be made ready for shipping within 24 hours.

Because of current order peaks our lead-time will increase temporarily to 6-12 working days for e-chain systems®. We are working intensively on a fast improvement.

igus® contact +49 (0) 2203-9649-0 Send e-mail to igus®

myigus myCatalog

Press releasesPress contactInclude into the press distribution list

No minimum order value
700 - 2000 Delivery+Consultation Delivery from 24h* Free samples

More than 100,000 products available! Delivery and consultation Mon-Fri from 7am-8pm and Sat from 8am-12pm!

Newsletter Registration
Terms and Conditions Imprint General Information Data Privacy Protection Declaration